cancel
Showing results for 
Search instead for 
Did you mean: 

X-NUCLEO-IHM08M1 schematic question

luke514
Senior

I'm looking at a diagram of the X-NUCLEO-IHM08M1 and the manual states that you can select either 1 shunt or 3 shunts using jumpers J5 and J6.

By default, there is one shunt, but when tested with a multimeter, there is continuity between the two red points in the photo:

luke514_0-1779783310650.png


With the multimeter, I should be getting a reading of 10 mΩ on the tin, right? And between the tin and the other plate?

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

At a glance through the schematics of the X-NUCLEO-IHM08M1, you will find on J6 (similar for J5) the two signals Vshunt_2 and Vshunt_3, each of which leads to a shunt with 10mΩ. All of these shunts are connected to GND, so you should measure 20mΩ between the signals - which ordinary multimeters usually cannot distinguish.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
Peter BENSCH
ST Employee

At a glance through the schematics of the X-NUCLEO-IHM08M1, you will find on J6 (similar for J5) the two signals Vshunt_2 and Vshunt_3, each of which leads to a shunt with 10mΩ. All of these shunts are connected to GND, so you should measure 20mΩ between the signals - which ordinary multimeters usually cannot distinguish.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Andrew Neil
Super User

@luke514 wrote:

I should be getting a reading of 10 MΩ on the tin, right? 


Did you mean MΩ - or mΩ  ?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

You're right, I made a mistake... it's

Thanks for clarifying that.

So, correct me if I’m wrong, but if I want three shunts I remove the current solder and reposition it in the opposite direction (from vertical to horizontal, as shown in the photo in the first post)

Yes, but not only for J6, but also for J5.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.