2018-11-02 11:51 PM
Hello there,
I am currently analyzing the STUSB1602 chip and the P-NUCLEO-USB002 eval kit. I have come across a topic I am not fully certain about. Its the SPI interface for the BMC communication. I cannot understand either it is necessary in all applications, or only if I want to exchange some specific data between devices over CC line? For example, if I intend to create a sink only device, so I have to connect the SPI lines and provide any data from the MCU? I would appreciate all help.
Solved! Go to Solution.
2018-11-12 7:36 AM
2018-11-12 11:46 PM
Hello Benoit,
So my adventures with the P-NUCLEO-USB002 ended after I have connected external 20 V supply to the CN12 port. The whole circuit was not powered up at that instance. I have only heard the typical "crack" of a frying IC and then came the smell... With the corner of my eye I have seen the display of the lab AC adapter, on which some current was indicated for a moment. Looking at the schematics of the P-NUCLEO-USB002 I am not sure what went wrong. The + terminal of the CN12 goes to the INA199A1DCK chip, which has 26 V differential input. Also I did not swap terminals polarity, I am certain. INA199A1DCK must have transferred the 20V input to the output since all circuit is dead (both base Nucleo board and the USB C hat).
Benoit- Any chance you have this P-NUCLEO-USB002 for spare? Also, do you have any clue what went wrong here?
2018-11-13 3:43 AM
V, Hello Lukasz,
I'm afraid in order to use the board with power management (over 5V I mean), it does not work this way. The port in the back of the blue board is used for that but it is quite complex to set-up. The protocol manages accurately the voltage transition (from 5V to the agreed voltage). This is why 20V can't be plugged directly. I'm going to ship to you:
- an STEVAL-ISC004V1 that you can use as a 5V, 9V, 12V, 15V, 20V SOURCE / power supply, and in order to read SINK capabilities,
- and a replacement P-NUCLEO-USB002 that I advise to use as a "sniffer" (and not as a SOURCE), in order to read attached device role and profiles.
rgds,
Benoit
2018-11-13 3:49 AM
2018-11-14 4:39 AM
Hello Benoit,
I started testing the p-nucleo-usb002 with STEVAL-ISC004V1 right ahead. I was able to choose all available profiles but 5th:
P-NUCLEO-USB00x Demo v1.0.4
Console v0.4
Type help for a list of commands.
STMicroelectronics
Copyright (c) 2017 - All Rights Reserved.
>
*** [1] attached on CC2 (Sink)
*** [1] selected cap #1
s 1
Role: Sink - Explicit contract CC2 Profile 1 5.00V
>r 1 1
Requested 1 : 5.00V 3.00A
>
*** [1] selected cap #1
r 1 2
Requested 2 : 9.00V 3.00A
>
*** [1] selected cap #2
r 1 3
Requested 3 : 12.00V 3.00A
>
*** [1] selected cap #3
r 1 4
Requested 4 : 15.00V 3.00A
>
*** [1] selected cap #4
r 1 5
Requested 5 : 20.00V 2.25A
>
*** [1] detached
*** [1] attached on CC2 (Sink)
*** [1] selected cap #1When I connected the STREF-SCS001V1 to the STEVAL-ISC004V1, I got 20 V output, so this one works. What could be the case for p-nucleo-usb002?
2018-11-14 9:49 AM
Hi Lukasz,
very strange. working properly on my side. Which Power supply are you using to power STEVAL-ISC004V1 (SOURCE)? We recommend 24V DC to supply the DC/DC from the board and ensure clean 20V output. What might happen is that the DC/DC can't regulate properly at 20V, so either the SOURCE and the SINK may terminate the connection as not in line with the expected contract (20V) +/- OVLO/UVLO (usually 10% if I remember well). In this case, the 2 different SINKs may have different settings, explaining the difference.
rgds,
Benoit
2018-11-14 9:52 AM
2018-11-14 9:52 AM
2018-11-16 5:31 AM
Hello Benoit,
I just tried connecting 25 V to the STEVAL-ISC004V1. I was able to successfully switch to the last profile like you now using the p-nucleo-usb002. Probably voltage drop on the DC-DC converter was to high. Thank you for help.
Btw, I wanted to test how would the p-nucleo-usb002 act after I connect a generic USB charger to it, like this: https://allegro.pl/ladowarka-gc-usb-c-45w-laptopa-acer-asus-dell-hp-i7527595704.html (frogive the polish language). Anyways, the specification says that it should support the following profiles: 5V-3A, 9V-3A, 12V-3A, 15V-3A, 20V-2.25A.
After I connected it to the p-nucleo-usb002 connector, I havent seen any event in the terminal nor on the leds- like the p-nucleo-usb002 didnt notice this charger at all. What could be the case here, since it is possible to charge a mobile phone using this USB C charger?
2018-11-16 6:48 AM
Hi Lukasz,
no reason, it should connect properly. Have you tried connecting the STREF-SCS001V1 to this USB charger? it should connect at 20V automatically if I cross properly the PDO from both devices.
benoit
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.