2019-08-21 8:24 AM
Hi all,
I'm trying to use the X-NUCLEO-PLM01A1 expansion board with the NUCLEO-F401RE board. I've been following the instructions to bring it up, and one of the instructions was to install the STSW-PLM2GUI to be able to interface the boards with the EVALKITST7580-1 GUI. However, after installing the software the GUI looks different from the one shown in the datasheet, and any attempts to connect to the board results in the message "SM : Status Message not received, check for connections". Additionally, running the P2P demo code on the board causes a "Warning: non STX character received" message to appear repeatedly, although the data is readable over PuTTY. I've noticed the version of the GUI is ST7580 GUI R21 (2017/08/04) while the datasheet shows X-NUCLEO-PLM01A1-7580 GUI R20 (2017/05/18) which I have not been able to find anywhere online. Can someone help me find the correct version of the GUI or get the one I have to work properly?
2020-05-08 5:33 AM
Hi all,
I had the same problem. I made the following adjustments:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.