2019-03-25 10:26 AM
Hello,
I am using the first generation STEVAL-STLKT01V1, I have complied and downloaded the BLE_SampleApp onto the board. I cannot connect to the board using the app.
Below are the debug output from the consol
STMicroelectronics STLBLE1:
Version 2.0.0
SensorTile
OK Temperature Sensor2
OK Pressure Sensor
Enabled Temperature Sensor2
Enabled Pressure Sensor
(HAL 1.8.2_0)
Compiled Mar
GATT_Init failed
Error while adding HW Service W2ST
Error while adding Config Service W2ST
Many thanks,
Sam
2019-04-08 12:29 AM
Hi Sam,
Tested STEVAL-STLKT01V1 with STSW-STLKT01 v2.0.0
and it worked properly for me.
Below would be the output prints:
STMicroelectronics STLBLE1:
Version 2.0.0
SensorTile
OK Humidity Sensor
OK Temperature Sensor1
OK Temperature Sensor2
OK Pressure Sensor
Enabled Humidity Sensor
Enabled Temperature Sensor1
Enabled Temperature Sensor2
Enabled Pressure Sensor
(HAL 1.8.2_0)
Compiled Apr 8 2019 15:24:19 (IAR)
Send Every 500mS Temperature/Humidity/Pressure
Debug Connection Enabled
Debug Notify Trasmission Enabled
SERVER: BLE Stack Initialized
Board type=SensorTile HWver=49, FWver=7.1.e
BoardName= STLB200
BoardMAC = c0:78:3e:34:51:38
HW Service W2ST added successfully
Config Service W2ST added successfully
2019-04-17 9:10 AM
Turns out i have a broken board
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.