Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STUSB1600 (USB Type-C) and USB OTG

I'm trying to understand how I can use a USB Type-C connector together with the STM32MP1 USB OTG peripheral.So obviously I want to use the port in dual role configuration. I want to use the STUSB1600 for that because it takes care of the power source...

arturo182 by Associate II
  • 13055 Views
  • 8 replies
  • 0 kudos

SPBTLE-1S, GPIOs

Hello,I am looking to prototype a project. I will need I2C, SPI and UART.  I2C for some ST sensors/gas gauge, SPI for sd card and UART for RS485.  Is it possible to use SPBTLE-1S, to run both host applications and bluetooth.  Thanks for your help

Sam Ho by Associate II
  • 2116 Views
  • 2 replies
  • 0 kudos

What is the HAL configuration on the STM34F4 discovery for playing wav files converted to 16b hex through the CS43L22 vis I2S?

I'm trying to get the discovery board to play a wav file that I've converted to an array of 16b hex values. So far, I have only been able to output an obnoxious noise. I have tried keeping the registered in the CS43L22 all at default.I have tried con...

TNixo by Associate
  • 827 Views
  • 0 replies
  • 0 kudos

Resolved! [STUSB4500] writing NVM memory on STUSB4500 procedure?

Dear I want to update the NVM memory on the STUSB4500. May I know the procedure of this, I download the STUSB003 SW lib. it not showing how to write NVM. My guessupdate the register call function void nvm_flash(uint8_t Port)reset Am I right?? also wh...

vlee by Associate II
  • 1733 Views
  • 1 replies
  • 1 kudos

STEVAL-STLKT01V1 GATT_Init failed

Hello,I am using the first generation STEVAL-STLKT01V1, I have complied and downloaded the BLE_SampleApp onto the board. I cannot connect to the board using the app.Below are the debug output from the consolSTMicroelectronics STLBLE1:    Version 2...

Sam Ho by Associate II
  • 1038 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.