2019-12-18 3:09 AM
2019-12-26 7:10 PM
USB, RS-485, and CAN on the STEVAL-IDP004V1 are provided for more flexibility, which can be used for data exchange with additional units and with multiple sensor connections on the STEVAL-IDP003V1.
In the evaluation firmware, PC_Communication_USB project is to manage command decoding and data exchange between the STEVAL-IDP004V1 and a PC.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.