Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.
STEVAL-IDB007V1- Virtual COMI have reprogrammed the STM32L151CB on board with the following two file:C:\Program Files (x86)\STMicroelectronics\BlueNRG GUI 3.1.0\Firmware\STM32L1_prebuilt_images\DFU_Bootloader.hex C:\Program Files (x86)\STMicroelectro...
Hello,my name is Clément and I am a student and new to STM. I have experience in programming 8 bit PIC microcontroller in C/MPLAB X and I also have worked with a BeagleBone Black and C++/Eclipse.For a project I'd like to use a STM32 microcontroller w...
Hi, I've download and install the STSW-BLUENRG1-DK (V3.1.0) :https://www.st.com/en/embedded-software/stsw-bluenrg1-dk.htmlUnfortunatly, when installation finished, i didn't see any library folder where i can find all the include file (bluenrg1_stack....
Hello,I want to add acknowledge funtionality to the Mesh Lighting demo from ST.What do I have to do to activate this and which funtion do I need to call to send an acknowledge-signal?Also for visibility, I'd like to have a LED flash when the sending ...
Hi Sir,Here we are looking for a development to test the BLE232 module. There are two boards. Top board (BLE232) is stacked on the development (BlueNRG-2). Ss it available in ST. We found this image in the china market. Can we buy this development bo...
Hi,I m trying to interface X-NUCLEO-NFC01A1 with BlueNRG2. After googling around I found projects and codes for stm32 based nucleo boards, but couldn't find anything for BlueNRG2.Can you provide me the project or source code for the same?
I have a development board (STM32F2(4)0x ETH CARD made by Mikroelectronica that has an STM32F407VG MCU and a built-in PHY using the LAN8720A. I cannot seem to figure out what I need to set in Cube MX in order to get the Ethernet port to connect to an...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.