2021-05-10 3:05 PM
I have an STEVAL-IDB005V1 that will not enumerate as a serial port on either Windows 7 or Windows 10 so I can't use the GUI to update the Bluetooth stack. Any help would be appreciated.
I also have an STEVAL-IDB006V1 that does enumerate but does not advertise. Any help would be appreciated.
Thanks
2021-05-10 11:44 PM
>I have an STEVAL-IDB005V1 that will not enumerate as a serial port on either Windows 7 or Windows 10
It the board powered on? Check the power option.
Do you see anything from the Device Manager? Try to flash the onboard STM32L from the JTAG connector, with the prebuilt VCOM firmware image in DK.
>I also have an STEVAL-IDB006V1 that does enumerate but does not advertise
I guess you need to configure it to advertise accordingly. Can you connect it with the GUI?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.