2020-03-11 3:44 AM
I try to understand the logic of the kit.
I open STSW-BLUETILE-DK 1.2.0->Project->BLE_Examples->BLE_Beacon
And I see in the main routine
while (1)
{
/* BlueNRG-1 stack tick */
BTLE_StackTick();
/* Enable Power Save according the Advertising Interval */
#if ST_USE_OTA_SERVICE_MANAGER_APPLICATION
if (!isPlugged)
{
if (GPIO_ReadBit(GPIO_Pin_11) == Bit_SET)
BlueNRG_Sleep(SLEEPMODE_NOTIMER, WAKEUP_IO11, (WAKEUP_IOx_LOW << WAKEUP_IO11_SHIFT_MASK));
else
BlueNRG_Sleep(SLEEPMODE_NOTIMER, WAKEUP_IO11, (WAKEUP_IOx_HIGH << WAKEUP_IO11_SHIFT_MASK));
}
#else
BlueNRG_Sleep(SLEEPMODE_NOTIMER, 0, 0);
#endif
}But where is a periodic data retrieving from the sensors? Where is a beacon updating and advertising? Should I implement it by myself?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.