Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPIRIT1 TX by using GPIO PIN for OOK

Hello. I want to use OOK modulation based on GPIO pin. Datasheet says it is capable of doing it, but it is nearly impossible to understand how to set this up.Could Some one provide explanation and register values and settings in order for GPIOX to co...

Linas L by Senior II
  • 725 Views
  • 0 replies
  • 0 kudos

STEVAL-BCN002V1B question.

I try to understand the logic of the kit.I open STSW-BLUETILE-DK 1.2.0->Project->BLE_Examples->BLE_BeaconAnd I see in the main routinewhile (1) { /* BlueNRG-1 stack tick */ BTLE_StackTick();   /* Enable Power Save according the Advertising In...

BlueNRG-2 pins for UART comms

I have a custom-built board with a BlueNRG-2 chip on it. The BlueNRG-2 chip is flashed with the UART version of the binary provided in the STM32CubeExpansion_BLE2_V1.0.0 package.Can anyone provide me the pins that the BlueNRG-2 uses for its UART comm...

SBukh.1 by Associate II
  • 610 Views
  • 0 replies
  • 0 kudos

IDB008v2: No ST-LINK detected

Hello everyone,I just got an IDB008v2 evaluation board and I'm having some issues setting it up and programming it.I can flash some demo programs from the BlueNRG-2 Navigator, which works (Tera Term receives the print messages and BLE scanner app see...

RCler.11 by Associate
  • 2214 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.