2018-02-22 1:40 PM
Hi,
I'm working with SPWF04SA using UART in a custom project. I have a issue making calls to NTP server. I've tried with several servers, but the behaviour is the same, I can't get response.
This is what I send and what I receive:
+WIND:1:Poweron:170216-fd39c59-SPWF04S
+WIND:13:Copyright (c) 2012-2017 STMicroelectronics, Inc. All rights Reserved:SPWF04SA +WIND:0:Console active +WIND:3:Watchdog Running:20 +WIND:32:WiFi Hardware Started +WIND:21:WiFi Scanning +WIND:35:WiFi Scan Complete:00 +WIND:19:WiFi Join:BB:AA:EE:AA:50:40 +WIND:25:WiFi Association successful:MyNetwork +WIND:51:WPA Handshake Complete +WIND:24:WiFi Up:0:192.168.50.207 AT+S.SOCKON=ntp.inrim.it,123,NULL,u AT-S.On:193.204.114.105:0 AT-S.OK AT+S.SOCKW=0,48 AT-S.ERROR:60:IP not ready to send +WIND:24:WiFi Up::fe80:0:0:0:280:e1ff:febd:f6c5 +WIND:84:NTP Server delivery:2018.2.22:4:21.1.53And, It is interesting this line:
AT-S.ERROR:60:IP not ready to send
This apears 40 seconds after calling NTP server.
And, this another line is also interesdtin too:
+WIND:84:NTP Server delivery:2018.2.22:4:21.1.53
Well, as I can see, efectivily, the wifi module can get a NTP update, but, where is the response packet that I requested with the UDP socket connection to port 123?
I was expecting something like:
+WIND:55: ...
What am I doing wrong?
Regards
AR
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.