2018-04-13 6:15 AM
We are using SPWF04 recently and found this module when running at standby mode would draw around >1mA current rather than uA level mentioned in the datasheet (it actually comes to uA for a couple of seconds and turns to 1.7mA after). May I know if SPWF04 could be a compatible replacement for SPWF01, any notice/tips for Hardware redesign, IO config or AT comment settings? Thanks.
2018-04-13 10:40 AM
Dear,
could you please try setting standby_time=240? You should see the current consumption in the uA level for about 4 minutes.
Please do not use values greater than 255 as we found a mismatch with what stated in the user manual. The behavior will be aligned to user manual in the next FW release.
Regards
Elio
2018-04-13 2:03 PM
Hi Elio,
This is really helpful. I will try and get back. May I know if there is an estimated timing for the next FW and UM? Thank you so much for your kind help. Have a good one.
2018-04-15 10:04 PM
Hi
Elio,
We have done a further test with shorter time-out period (240 seconds or even 100) and the module behaves the same as the current draw still remains around 1.5 mA in standby mode... Could you please provide further tips. Thank you so much.
2018-04-16 10:02 AM
Hi,
all GPIOs are put in high impendence when the module is rebooted in standby mode (AT+S.PMS=3) and you should expect a current consumption around 43uA regardless what is connected to the GPIOs. When the standby time expires or GPIO[6] is moved then the SPWF04 is woken up and the current consumption will increase to the level of your specific configuration.
I kindly ask you:
- to dump and send me your configuration (AT+S.GCFG) and status (AT+S.STS) just before issuing the PMS=3 command;
- to verify the current consumption only comes from pin24 (Vcc) of SPWF04.
2018-04-16 6:58 PM
Hi Elio,
Yes. We leave all unused GPIOs open/floating and even tried to add RC at GPIO[6]. But the standby current is still holding at uA only around 4s and raise up to 1.7 mA. Please see the status query as you required below. Your comment and advice are much appreciated. Thanks a lot.
AT+S.GCFG AT-S.List AT-S.Var:nv_manuf=ST AT-S.Var:nv_model=SPWF04SA AT-S.Var:nv_serial=3817Z22816 AT-S.Var:nv_wifi_macaddr=00:80:E1:BD:FE:F1 AT-S.Var:standby_time=10 AT-S.Var:standby_enabled=0 AT-S.Var:sleep_enabled=0 AT-S.Var:etf_mode=0 AT-S.Var:blink_led=1 AT-S.Var:ext_volume=3 AT-S.Var:ramdisk_memsize=16 AT-S.Var:aes128_key=00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00 AT-S.Var:user_desc=anonymous AT-S.Var:python_script=3:/uPython_test.py AT-S.Var:python_memsize=32 AT-S.Var:console_enabled=1 AT-S.Var:console_speed=115200 AT-S.Var:console_hwfc=0 AT-S.Var:console_echo=1 AT-S.Var:console_errs=2 AT-S.Var:console_winds=2 AT-S.Var:console_verbose=1 AT-S.Var:console_repeater=0x21 AT-S.Var:console_delimiter=0x2C AT-S.Var:console_wind_off_low=0x00000000 AT-S.Var:console_wind_off_medium=0x00000000 AT-S.Var:console_wind_off_high=0x00000000 AT-S.Var:wifi_tx_msdu_lifetime=0 AT-S.Var:wifi_rx_msdu_lifetime=0 AT-S.Var:wifi_operational_mode=0x00000011 AT-S.Var:wifi_beacon_wakeup=1 AT-S.Var:wifi_beacon_interval=100 AT-S.Var:wifi_listen_interval=0 AT-S.Var:wifi_rts_threshold=3000 AT-S.Var:wifi_ssid=53:54:54:65:73:74:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00 AT-S.Var:wifi_ssid_len=6 AT-S.Var:wifi_txfail_thresh=5 AT-S.Var:wifi_dtim_period=1 AT-S.Var:wifi_add_tim_ie=0 AT-S.Var:wifi_region=1 AT-S.Var:wifi_ht_mode=1 AT-S.Var:wifi_channelnum=6 AT-S.Var:wifi_opr_rate_mask=0x003FFFCF AT-S.Var:wifi_bas_rate_mask=0x0000000F AT-S.Var:wifi_mode=1 AT-S.Var:wifi_auth_type=0 AT-S.Var:wifi_atim_window=0 AT-S.Var:wifi_powersave=0 AT-S.Var:wifi_tx_power=18 AT-S.Var:wifi_rssi_thresh=0 AT-S.Var:wifi_rssi_hyst=0 AT-S.Var:wifi_ap_idle_timeout=120 AT-S.Var:wifi_beacon_loss_thresh=10 AT-S.Var:wifi_priv_mode=0 AT-S.Var:wifi_wep_keys[0]=00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00 AT-S.Var:wifi_wep_keys[1]=00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00 AT-S.Var:wifi_wep_keys[2]=00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00 AT-S.Var:wifi_wep_keys[3]=00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00 AT-S.Var:wifi_wep_key_lens=00:00:00:00 AT-S.Var:wifi_wep_default_key=0 AT-S.Var:wifi_wpa_psk_raw=00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00 AT-S.Var:wifi_wpa_psk_text= AT-S.Var:wifi_eap_identity=identity AT-S.Var:wifi_eap_anon_identity=mailto:anonymous@identity.org
AT-S.Var:wifi_eap_passwd=password AT-S.Var:wifi_eap_type=0 AT-S.Var:wifi_eap_skip_datechecks=0 AT-S.Var:wifi_wps_walk_time=120 AT-S.Var:wifi_wps_pin=1234567 AT-S.Var:ip_sock_memsize=1 AT-S.Var:ip_sock_threshold=0 AT-S.Var:ip_dhcp_lease_time=120 AT-S.Var:ip_macfilter=00:00:00:00:00:00 AT-S.Var:ip_num_clients=5 AT-S.Var:ip_allow_port_scans=1 AT-S.Var:ip_use_v6=1 AT-S.Var:ip_use_dhcpd=1 AT-S.Var:ip_use_httpd=1 AT-S.Var:ip_use_tftpd=1 AT-S.Var:ip_use_dhcpc=2 AT-S.Var:ip_hostname=iwm-BD-FE-F1 AT-S.Var:ip_apdomainname= AT-S.Var:ip_apredirect=firstset.html AT-S.Var:ip_ipaddr=192.168.0.50 AT-S.Var:ip_netmask=255.255.255.0 AT-S.Var:ip_gw=192.168.0.1 AT-S.Var:ip_dns1=208.67.222.222 AT-S.Var:ip_dns2=208.67.220.220 AT-S.Var:ip_local=0:0:0:0:0:0:0:0 AT-S.Var:ip_dns1v6=0:0:0:0:0:0:0:0 AT-S.Var:ip_dns2v6=0:0:0:0:0:0:0:0 AT-S.Var:ip_dhcp_timeout=20 AT-S.Var:ip_ntp_server1= AT-S.Var:ip_ntp_server2= AT-S.Var:ip_ntp_refresh=3600 AT-S.Var:ip_ntp_startup=1 AT-S.Var:ip_mdns_domain_name=SPWF04S-Default AT-S.Var:ip_mdns_device_name_ttl=120 AT-S.Var:ip_mdns_services_name=SPWF04S-WebSrv SPWF04S-TFTPSrv AT-S.Var:ip_mdns_services_prot=_http._tcp _tftp._udp AT-S.Var:ip_mdns_services_keys=dev1 dev2 AT-S.Var:ip_mdns_services_vals=number1 number2 AT-S.Var:ip_mdns_services_port=80 69 AT-S.Var:ip_mdns_services_ttl=120 60 AT-S.Var:ip_mdns_startup=01:01 AT-S.OK AT+S.STS AT-S.List AT-S.Var:build=171117-0328fe3-SPWF04S AT-S.Var:fw_version=1.1.0 AT-S.Var:boot_version=1.0 AT-S.Var:var_version=2 AT-S.Var:free_heap=46072 AT-S.Var:min_heap=43368 AT-S.Var:system_time=946684942 AT-S.Var:system_uptime=63 AT-S.Var:system_sleeptime=0 AT-S.Var:reset_reason=2 AT-S.Var:startup=0 AT-S.Var:random_number=660795666 AT-S.Var:gpio_enable=0x0000 AT-S.Var:app_fs=1 AT-S.Var:ram_fs=1 AT-S.Var:user_fs=0 AT-S.Var:extvol_fs=0 AT-S.Var:nv_power_cycles=1 AT-S.Var:nv_wdog_resets=0 AT-S.Var:nv_reset_cycles=4 AT-S.Var:wifi_state=5 AT-S.Var:wifi_own_macaddr=00:80:E1:BD:FE:F1 AT-S.Var:wifi_bssid=00:00:00:00:00:00 AT-S.Var:wifi_aid=0 AT-S.Var:wifi_channelnum=0 AT-S.Var:wifi_sup_rate_mask=0x003FFFCF AT-S.Var:wifi_bas_rate_mask=0x00000000 AT-S.Var:wifi_chan_activity=0x00001FFF AT-S.Var:wifi_max_tx_power=18 AT-S.Var:wifi_gf_mode=0 AT-S.Var:wifi_reg_country=AU AT-S.Var:wifi_dtim_period=0 AT-S.Var:wifi_num_assoc=0 AT-S.Var:ip_from_AutoIP=0 AT-S.Var:ip_ipaddr=0.0.0.0 AT-S.Var:ip_netmask=0.0.0.0 AT-S.Var:ip_gw=0.0.0.0 AT-S.Var:ip_dns1=0.0.0.0 AT-S.Var:ip_dns2=0.0.0.0 AT-S.Var:ip_linklocal=0:0:0:0:0:0:0:0 AT-S.Var:ip_local=0:0:0:0:0:0:0:0 AT-S.Var:ip_dns1v6=0:0:0:0:0:0:0:0 AT-S.Var:ip_dns2v6=0:0:0:0:0:0:0:0 AT-S.OK2018-04-19 3:26 AM
Hi Elio,
We are still keen to know your kind comment and advice regarding to this issue. The feedback is important to the decision making on whether to keep ST 04 module in our future products. Thank you so much for your great support.
2018-04-19 9:33 AM
Hello,
we are trying to figure out why your sample is consuming such amount of current.
I'll update you ASAP.
Elio
2018-04-25 5:13 PM
Hi Elio,
May I know if you have any progress and further comment on this case. BTW, the main board for this test is based on STEVAL-IDW001V1, will try
X-NUCLEO-IDW04A1 later.
Thank you so much.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.