2018-04-25 9:07 AM
Hi,
I want to connect to the wifi board XNUCLEO-IDW04A1 with my nucleo stm32l476RG developpment board. However I am getting a strange behaviour similar to what is posted on
https://community.st.com/0D50X00009XkYRKSA3
except that I get the problem at the beginning of the example Client_Socket in the x-cube-wifi1_firmware.V3.1.1. I used the latest firmware SPWF04S-171117-0328fe3-Full.hex for the wifi board. The program get stucked at line 433 of wifi_interface.cwhile(IO_status_flag.WiFi_WIND_State!= WiFiPowerDown);//Till +WIND:38:WiFi Powered Down arrives
Thank you
/********************************************************
* * * X-CUBE-WIFI1 Expansion Software v3.1.1 * * X-NUCLEO-IDW0xx1 Wi-Fi Configuration. * * Client-Socket Example * * * *******************************************************/Do you want to setup SSID?(y/n):n
Module will connect with default settings.
/**************************************************************
* Configuration Complete * * Port Number:32000, Protocol: TCP/IP * * Please make sure a server is listening at given hostname * *************************************************************/Initializing the wifi module...Build Configuration:
Nucleo: NUCLEO-L476RGX-Nucleo: X-NUCLEO-IDW04A1Interface: SPI>> Configuration Failure no 2
<<WIND 7, status 0<<WIND 1, status 0
<<WIND 13, status 0
<<WIND 3, status 0
<<WIND 0, status 0
<<WIND 32, status 3
>>AT+S.SCFG
<<OK
>>AT+S.FCFG
<<OK
>>AT+S.WCFG
<<OK
>> Configuration Failure no 2
<<WIND 7, status 0<<WIND 1, status 0
<<WIND 13, status 0
<<WIND 3, status 0
<<WIND 0, status 0
<<WIND 32, status 3
WiFi Initialised and Ready..
>>AT+S.WIFI
<<OK
nullWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.