2018-03-12 4:31 AM
Hello I have a SPWF04 Wifi Module and I've tried to use the SPI interface to communicate with it but without success..
Could anyone help me to configure the SPWF04 module in spi mode?here are the my (unsuccesful) steps:
step 1: phisycal pull-up on GPIO9 step 2: configure host (STM32L476) pin as EXTI Line on Falling edge (connected to SPWF04 GPIO9) step 3: reset Wifi Module from my host by driving down nRESET pin, wait some hundreds of milliseconds, driving hi nRESET pin. step 4: every time the host receives an Exti, read 5 bytes over SPI(according SPI packet format in UM2114 at page 11) to decode start message, kind of event, indication number, payload lenght step 5: check first received byte and verify that his value is 0x02at this point I have to stop because first byte is not 0x02 as indicated in UM2114.
SPI Host interface is configured with:
frame format = MotorolaFirst bit = MSB FirstData Size = 8bit
Baud Rate = 8Mbit/sCPOL = LowCPHA = 1st Edgethe DS lascks some information with this regard. What am I doing wrong?
Thank you
Regards
##spi ##spwf04saWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.