2018-03-06 9:01 AM
Hi, I'm looking to do some timing specific code with the Bluenrg MS
It is running as a peripheral, and once a connection is established, we send an update connection request to the master, and get a response saying is was accepted.
The problem I'm running into, is what is the exact connection interval the master will use?
In the request we supply a min and max value (10ms to 20ms, 0 slave latency), but the response only says that these parameters were accepted.
Is there a procedure, or ACI type command that we can use to query the connection interval actually being used?
#ble #bluenrg2018-03-09 6:35 AM
Hi,
you can get that information by using the HCI_Event_CB() callback. The latter is called whenever you get an event from the BlueNRG-MS chip. If you need the actual connection interval chosen by the Central device, you can handle the EVT_LE_META_EVENT, where you can read out this information as the interval parameter of the evt_le_connection_complete data structure.Below I've highlighted the part of code(uint16_t conn_interval = cc->interval)that you need to add to your existing HCI_Event_CB() callback function.
void HCI_Event_CB(void *pckt)
{
hci_uart_pckt *hci_pckt = pckt;
/* obtain event packet */
hci_event_pckt *event_pckt = (hci_event_pckt*)hci_pckt->data;
if(hci_pckt->type != HCI_EVENT_PKT)
return;
switch(event_pckt->evt){
case EVT_DISCONN_COMPLETE:
{
GAP_DisconnectionComplete_CB();
}
break;
case EVT_LE_META_EVENT:
{
evt_le_meta_event *evt = (void *)event_pckt->data;
switch(evt->subevent){
case EVT_LE_CONN_COMPLETE:
{
evt_le_connection_complete *cc = (void *)evt->data;
/* THIS IS WHERE YOU CAN GET THE ACTUAL CONNECTION INTERVAL */
uint16_t conn_interval = cc->interval;
GAP_ConnectionComplete_CB(cc->peer_bdaddr, cc->handle);
}
break;
}
}
break;
typedef __packed struct _evt_le_connection_complete{
uint8_t status;
uint16_t handle;
uint8_t role;
uint8_t peer_bdaddr_type;
tBDAddr peer_bdaddr;
uint16_t interval;
uint16_t latency;
uint16_t supervision_timeout;
uint8_t master_clock_accuracy;
} PACKED evt_le_connection_complete;
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
Best regards,
Antonio
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.