2017-09-15 7:50 AM
Hi,
I am using the SPWF04 and want to update the filesystem via UART.Is it possible?For the SPWF01 there is the command AT+S.HTTPDFSWRITE but thats not working with the SPWF04.
I've read in another post that it might be possible with FLASHER/ST-LINK (wired UART/SWD) but I can't find any further informations.
Thanks for your help!
2017-09-15 9:24 AM
In the SPWF04 the filesystem is stored in the STM32's internal flash, hence you can use the STM32 Flash loader demonstrator (go to
and search for FLASHER-STM32 or STM32 Flash loader demonstrator).The starting address of the filesystem is:
- 0x8100000 for Application Disk
- 0x8110000 for User Disk
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.