Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

smtp with SPWF04SA

Posted on September 14, 2017 at 23:18Hello,I'm working with an SPWF04SA. I set up the Wi-Fi connection correctly, it responds well to ping, but I can not send an email.I have tried several things, and I only get a certificate 5 error (the common nam...

SPWF04 filesystem update via UART

Posted on September 15, 2017 at 16:50Hi,I am using the SPWF04 and want to update the filesystem via UART.Is it possible?For the SPWF01 there is the command AT+S.HTTPDFSWRITE but thats not working with the SPWF04.I've read in another post that it mig...

sensor tile & BlueNRG

Posted on September 01, 2017 at 11:39Hey Folks, i'm currently starting with developing applications for the SensorTile. I try to achieve so advertise a custom BLE Packet (like an AltBeacon Protocol). I found the hci_le.c header in de Middleware. It ...

BlueNRG-MS simultaneously Master&Slave

Posted on July 21, 2015 at 11:00Hello, i'm using aBlueNRG-MS module.I have a problem with this module. I can use it as Master and Slave, but i can't use it as Master&Slave simultaneously. Because after i create a connection with a slave module i can...

aci_hal_tone_start test

Posted on September 12, 2017 at 14:48Hello,I am trying to do a test with the bluenrg-1, I have connected 2 led's to different inputs, I am blinking those leds every second and they are working fine but when I try to use the aci_hal_tone_start( 0 ), ...

jampino by Associate III
  • 617 Views
  • 0 replies
  • 0 kudos

Receiving connections from two central devices

Posted on September 07, 2017 at 16:37My device works as peripheral in stack mode 2. This means it can handle connection from one central device only. I need to handle at least two central/master devices simultaneously. How can I do that? I suppose I...

grzegorz by Associate III
  • 670 Views
  • 1 replies
  • 0 kudos

WFDFPN8 (MLP8) 2x3mm land pattern

Posted on September 07, 2017 at 17:37Hi, I'm trying to design a PCB with the M95640-DRMF3TG (AKA M95128-A125) Serial EEPROM, and cannot find a land pattern for the part.  The best thing I can find is TN1171 (Technical Note), but it does not give any...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.