2014-05-26 7:18 AM
I have a SPWF01SA wifi module initially it is all good I communicate with him through a terminal. I do a reset control module (AT + CFUN = 1) then it always enters a reset mode and does not accept any command. How can we get out of this infinite loop reset.
#spwf01sa2014-05-26 7:54 AM
I think i did not get your question.
Take a look at boot pin. Is it high (2V5)? It means that inner STM32 is in boot mode, and, so, application into SPWF does not start...2014-05-27 4:27 AM
Hi,
Thank you for your reply, I have another question : is that there is a command to cancel for a period, asynchronous outputs sent by the module (''+ WIND: 21: WLAN Scanning'' or ''+ WIND: 35: Complete Scan''). I test this variable but no results ''wifi_print_scan_results'' .2014-05-27 6:35 AM
Hi,
unfortunatelly you have a very very old firmware. that variable does not exist since a long time...When the module is not connected, you cannot stop scan (unlee you use the ''at+s.wifi=0'' command), but... since FW Release 3.x on, there are 3 variables called wind_off_low/medium/high. Default values are 0x00000000s. It's a bitmask.- wind_off_low manages wind:0 to wind:31- wind_off_medium manages wind:32 to wind:63- wind_off_high manages wind:64 to wind:94 (wind_off_high[95] is reserved)Example:- ''at+s.scfg=wind_off_low,0x00200000'' hides wind:21- ''at+s.scfg=wind_off_medium,0x00000008'' hides wind:35- ''at+s.scfg=wind_off_high,0xFFFFFFFF'' hides wind:64 to wind:94I don't know if you want to stop scan, or only hide WINDs messages...We’re moving the ST Community to a new platform to give you a better and more reliable community experience.