Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPWF01SA ???

Posted on May 26, 2014 at 16:18I have a SPWF01SA wifi module initially it is all good I communicate with him through a terminal. I do a reset control module (AT + CFUN = 1) then it always enters a reset mode and does not accept any command. How can ...

Transmit power setting

Posted on May 20, 2014 at 22:46Back in the December 2013 version of UM1695, there was a command to set the transmitter power of the module:at+s.scfg=wifi_tx_power,42In the firmware that I have, I get the response ''ERROR: Unrecognized key'', and get...

CR95HF and STM32F4-discovery

Posted on May 21, 2014 at 16:20Hi,I'm trying to use MikroElektronika RFID Click (with a CR95HF embeded) as RFID Reader with a STM32F407VG.The CR95HF is connected to the STM32F4 by SPI. The driver and Lib provide by ST are working with STM32F1. It do...

SPBT2632C2A Module Communication

Posted on April 30, 2014 at 01:29Can the SPBT2632C2A module be setup to use SPI communications in an embedded application instead of UART?  Is a new firmware needed to accomplish this? Is there an example on how to set this up?

tidd by Associate II
  • 1655 Views
  • 3 replies
  • 0 kudos

STDP4020 Firmware Version Detect

Posted on April 04, 2014 at 00:05I am currently working a project to detect the version of STDP4020 firmware. I got all the data bytes of this firmware, can anybody give me some clue how to interpret them, particularly, which part tells the version ...

yao by Associate
  • 1428 Views
  • 1 replies
  • 0 kudos

BlueNRG reset mode

Posted on March 21, 2014 at 09:03Hi all, can you clarify which is the status of the BlueNRG pinin reset mode? Best Regards &Thank you

zhanfu4 by Associate II
  • 1146 Views
  • 1 replies
  • 0 kudos

Issues with SPWF01S wifi module

Posted on March 19, 2014 at 18:16I'm having some issues with the SPWF01S WiFi modules. I have tried putting in a technical support request, but haven't gotten much response in the last month. I was wondering if this would be an appropriate place to ...

SPIRIT1 / FDEV0 REGISTER ( PLL & DLL mode )

Posted on March 21, 2014 at 09:16Hi, What is the recommendation about the use of these two algorithms in the application? By default DLL is selected, I would like to understand if it is possible to use PLL mode or not. Any more detailed description ...

kaneie by Associate
  • 851 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.