2014-10-02 3:49 PM
Hi
What's the max bps/symbol-rate for SPWF01SA/SPWF01SC? thx #data-rate #symbol-rate #bps2017-02-01 3:43 AM
How does this answer relate to this:
Which is correct 40-50kB/s or 1Mbps (which is approx 100kB/s)?2017-02-01 10:22 AM
1MB is baudrate, 50KB is 'goodput' (amount of bits moved over the air in 1 seconds)
2017-02-02 12:46 AM
Ok. I tested 480600 baud/sec and that had around 40kB of data througput using http connections (I could not reach the same data rate using sockets, though).
So I assume that the 50kB/s limit is due to the firmware implementation. Do ST provide a firmware forSPWF01SA with SPI exposed for higher throughput? Or is it possible to change the firmware ourselves?
2017-02-02 3:10 AM
Please contact your local ST office, or distributor...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.