Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! POST large data with a single request

Posted on February 01, 2017 at 16:06Hi,I'm using a SPWF01SA1 module to send data from my application to a central server using POST requests.I need to transfer 64 kByte of binary data (application/octet-stream) using a single POST request as I want ...

Luca DC by Associate II
  • 2683 Views
  • 5 replies
  • 0 kudos

SPWF01: Module enters IP 192.168.0.50

Posted on January 30, 2017 at 16:55Hi,my modules are sometimes returning the IP address 192.168.0.50 since they already had another IP address from the access point. When they got the IP address 192.168.0.50, I can't connect to them via TCP anymore....

Strange behaviour with BlueNRG MS embedded

Posted on January 30, 2017 at 09:30Good morning everyone!I am actually working on two different electronics we created (different layout) both embedding Blue-NRG MS (FW 7.2.c).These electronics are embedding the Blue-NRG and also a STM32L acting as ...

SPWF01SA console1_delimiter update

Posted on January 23, 2017 at 17:23I have changed the delimeter to 0x23(#).I see in the parameters dump that it was changed but it is not accepted.Trying to use it returns argument missing error.Any ideas?I have to use the comma in my data.Thanks

../Src/stm32f1xx_it.c(193): error:

Posted on January 25, 2017 at 02:13My application receives data in usart1 and usart2 through interrupt.I generated the files in STM32CubeMX for keil.This error appears in the compilation:../Src/stm32f1xx_it.c(193): Error: # 20: identifier 'USART_IT_...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.