2017-08-30 3:52 PM
Hi Everyone,
I've been evaluating an SPWF01SC to see whether it's suitable to add web browser file transfer functionality and a control interface to an existing embedded (bare metal) project.
Host controller is an STM32F429 and files are stored on an SD card. Over USB this appears as a drive in Windows; I'd like something similar on the wifi interface. File sizes are < 2MB, most are a few KB so I can live with the relatively slow transfer rate (I've done some benchmarking using sockets).
As I'm not very familiar with web servers can the module can do this out-of-the-box with minimal coding (i.e. I'm missing something)? Is it better to bypass the web server and use sockets in the host (this is hard, I know)? Is the module just not suitable at all? Is there a better way?
Many thanks.
#spwf01scWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.