2014-12-02 4:48 AM
Hi all
First of all excuse my englishI'm trying to connect my SPWF01SA to an access point but I´m doing something wrong because I don't get access to the wifi net. I think that my configuration is correct but something happensthis is a log of the process:+WIND:1:Poweron (140225-02d76c4-SPWF01S)<CR><LF><CR><LF>+WIND:13:ST SPWF01SA1 IWM: Copyright (c) 2012-2014 STMicroelectronics, Inc. All rights Reserved.<CR><LF><CR><LF>+WIND:3:Watchdog Running<CR><LF><CR><LF>+WIND:0:Console active<CR><LF><CR><LF>+WIND:32:WiFi Hardware Started<CR><LF><CR><LF>+WIND:21:WiFi Scanning<CR><LF><CR><LF>+WIND:35:WiFi Scan Complete (0x0)<CR><LF><CR><LF>+WIND:21:WiFi Scanning<CR><LF><CR><LF>+WIND:35:WiFi Scan Complete (0x0)<CR><LF><CR><LF>+WIND:21:WiFi Scanning<CR><LF><CR><LF>+WIND:35:WiFi Scan Complete (0x0)<CR><LF>This is the config:AT&V<CR><LF># Dumping All Configuration Keys:<CR><LF># nv_manuf = ST<CR><LF># nv_model = SPWF01SA1<CR><LF># nv_serial = 0614D10309<CR><LF># nv_wifi_macaddr = 00:80:E1:FF:BC:7B<CR><LF># blink_led = 1<CR><LF># user_desc = anonymous<CR><LF># localecho1 = 1<CR><LF># console_uart = 1<CR><LF># console1_speed = 115200<CR><LF># console1_hwfc = 0<CR><LF># console1_enabled = 1<CR><LF># console2_speed = 115200<CR><LF># console2_enabled = 0<CR><LF># localecho2 = 1<CR><LF># console3_enabled = 0<CR><LF># console3_speed = 115200<CR><LF># localecho3 = 1<CR><LF># wifi_tx_msdu_lifetime = 0<CR><LF># wifi_rx_msdu_lifetime = 0<CR><LF># wifi_rts_threshold = 3000<CR><LF># wifi_ssid =46:54:45:2D:35:35:30:35
:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00<CR><LF># wifi_ssid_len = 8<CR><LF># wifi_mode = 1<CR><LF># wifi_auth_type = 0<CR><LF># wifi_rssi_thresh = 0<CR><LF># wifi_rssi_hyst = 0<CR><LF># wifi_ap_idle_timeout = 120<CR><LF># wifi_beacon_loss_thresh = 10<CR><LF># wifi_priv_mode = 0<CR><LF># wifi_wep_keys[0] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00<CR><LF># wifi_wep_keys[1] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00<CR><LF># wifi_wep_keys[2] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00<CR><LF># wifi_wep_keys[3] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00<CR><LF># wifi_wep_key_lens = 00:00:00:00<CR><LF># wifi_wep_default_key = 0<CR><LF># wifi_wpa_psk_raw = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00<CR><LF># wifi_wpa_psk_text =gtmq-dua
l<CR><LF># ip_use_dhcp = 1<CR><LF># ip_use_httpd = 1<CR><LF># ip_mtu = 1500<CR><LF># ip_hostname = iwm-FF-BC-7B<CR><LF># ip_apdomainname = captiveportal.net<CR><LF># ip_ipaddr = 192.168.0.50<CR><LF># ip_netmask = 255.255.255.0<CR><LF># ip_gw = 192.168.0.1<CR><LF># ip_dns = 192.168.0.1<CR><LF># ip_http_get_recv_timeout = 1000<CR><LF># ip_dhcp_timeout = 20<CR><LF>this is a scan to check that the module is seeing my netAT+S.SCAN<CR><LF>1:<HT> BSS F8:8E:85:C5:E1:5A CHAN: 01 RSSI: -87 SSID: 'MOVISTAR_E159' CAPS: 0411 WPA <CR><LF>2:<HT> BSS 00:1A:2B:B1:43:E8 CHAN: 01 RSSI: -90 SSID: '\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00' CAPS: 0411 WPA WPS <CR><LF>3:<HT> BSS 00:26:18:90:38:51 CHAN: 01 RSSI: -90 SSID: 'WebSTAR' CAPS: 0411 <CR><LF>4:<HT> BSS 9C:80:DF:87:80:EB CHAN: 02 RSSI: -90 SSID: 'Orange-80E9' CAPS: 0431 WPA WPA2 WPS <CR><LF>5:<HT> BSS 38:72:C0:DF:98:B6 CHAN: 03 RSSI: -90 SSID: 'luis-puy' CAPS: 0411 WPA <CR><LF>6:<HT> BSS 88:E3:AB:8F:42:C7 CHAN: 04 RSSI: -89 SSID: 'vodafone42BE' CAPS: 0411 WPA2 WPS <CR><LF>7:<HT> BSS 00:1A:2B:69:01:81 CHAN: 05 RSSI: -83 SSID: 'WLAN_9E' CAPS: 0411 WPA <CR><LF>8:<HT> BSS D0:AE:EC:C4:FD:08 CHAN: 06 RSSI: -71 SSID: 'WLAN_FD08' CAPS: 0C31 WPA WPS <CR><LF>9:<HT> BSS 00:25:69:A1:55:06 CHAN: 06 RSSI: -83 SSID: 'FTE-5505
' CAPS: 0411 WPA2 <CR><LF>10:<HT> BSS DC:53:7C:05:26:31 CHAN: 07 RSSI: -92 SSID: 'ONOC963' CAPS: 0411 WPA WPA2 WPS <CR><LF>11:<HT> BSS C0:3F:0E:FF:75:82 CHAN: 11 RSSI: -91 SSID: 'ONO7582' CAPS: 0411 WPA WPA2 <CR><LF>12:<HT> BSS 00:1A:2B:42:E4:98 CHAN: 11 RSSI: -85 SSID: 'JAZZTEL_18' CAPS: 0411 <CR><LF>13:<HT> BSS 00:1A:2B:5C:92:FB CHAN: 11 RSSI: -86 SSID: 'JAZZTEL_DA' CAPS: 0411 <CR><LF>Could you help me to see where is the mistake? The documentation is quite limitedThanks!2014-12-02 6:53 AM
Hi Victor,
''wifi_priv_mode = 0'' means no security. Is it correct?Try:at+s.scfg=wifi_priv_mode,2at&wat+cfun=1let me knowjps:140225-02d76c4 is an old version. I suggest to contact your local ST distributors, and update it.
2014-12-03 12:50 AM
Hi Gerardo
You are right! this is the mistake, now the module is connecting. Thanks for the quickly reply, and thanks for the advice, I´ll try to upgrade it.+WIND:1:Poweron (140225-02d76c4-SPWF01S)<CR><LF><CR><LF>+WIND:13:ST SPWF01SA1 IWM: Copyright (c) 2012-2014 STMicroelectronics, Inc. All rights Reserved.<CR><LF><CR><LF>+WIND:3:Watchdog Running<CR><LF><CR><LF>+WIND:0:Console active<CR><LF><CR><LF>+WIND:32:WiFi Hardware Started<CR><LF><CR><LF>+WIND:21:WiFi Scanning<CR><LF><CR><LF>+WIND:35:WiFi Scan Complete (0x0)<CR><LF><CR><LF>+WIND:19:WiFi Join: 00:25:69:A1:55:06<CR><LF><CR><LF>+WIND:25:WiFi Association with 'FTE-5505' successful<CR><LF><CR><LF>+WIND:51:WPA Handshake Complete<CR><LF><CR><LF>+WIND:24:WiFi Up: 192.168.1.11<CR><LF>Regards!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.