2017-01-04 12:52 AM
Hello,
I'am using this module to connecte my borad to Internet.
This module can create a mini AP so a user can connect its laptaop or smartphone to the SPWF01 and configure the WIFI connexion (SSID and pass).
I have no problème to connect to the mini AP with an old WIKO smartphone but I can't connect with a newer smartphone (Huawei P9 lite).
I have also discover a weird thing : If I first connect anything (old WIKO or laptop) to the mini AP, and then try with the P9 lite, it can connect to the mini AP.
thanks for your help.
Marc G
2017-02-08 10:26 AM
Hi Marc,
I suspect this is something added to miniAP after v3.5 (traffic information map bytes inside beacons). I can give you an updated FW, for a test. Send me a private message...
2017-02-10 3:43 AM
hello,
have you received my message with my Email address ?
regards.
Marc
2017-02-10 6:36 AM
yes
2017-10-13 12:22 AM
Hi Gerardo,
I have a similar problem with HUAWEI P8 Lite (2015).It connects and disconnects continuously in a loop.Can You help me?
I download and installed the app WIFI FIXER from Play store and I monitorized the thing.You can find the logs of the SPWF01 and of the app below. the firmware is 3.5 and the O.S. of the smartphone in Android 6.0.Best regards.
This is the log from the of the SPWF01:
+WIND:72:Station 5C:03:39:54:92:CC Disassociated:2
+WIND:28:Station 5C:03:39:54:92:CC Associated:0
+WIND:29:DHCP reply for 172.25.103.2/5C:03:39:54:92:CC
+WIND:72:Station 5C:03:39:54:92:CC Disassociated:2
+WIND:28:Station 5C:03:39:54:92:CC Associated:0
+WIND:29:DHCP reply for 172.25.103.2/5C:03:39:54:92:CC
+WIND:72:Station 5C:03:39:54:92:CC Disassociated:2
+WIND:28:Station 5C:03:39:54:92:CC Associated:0
+WIND:29:DHCP reply for 172.25.103.2/5C:03:39:54:92:CC
+WIND:72:Station 5C:03:39:54:92:CC Disassociated:2
+WIND:28:Station 5C:03:39:54:92:CC Associated:0
+WIND:29:DHCP reply for 172.25.103.2/5C:03:39:54:92:CC
+WIND:72:Station 5C:03:39:54:92:CC Disassociated:2
+WIND:28:Station 5C:03:39:54:92:CC Associated:0
And this is the log of the APP:
Build:1.0.5:1165
ALE-L216.02017-10-10 10:05:16: Network Check:
2017-10-10 10:05:20: Network check failed: Trying again2017-10-10 10:05:20: I/O Exception172.25.103.1:HTTP_FAIL:4007ms2017-10-10 10:05:20: Current dBm:-562017-10-10 10:05:20: WFMonitor Acquiring Wake Lock2017-10-10 10:05:20: Running Wifi Repair2017-10-10 10:05:20: Reassociating2017-10-10 10:05:20: WFMonitor Releasing Wake Lock2017-10-10 10:05:20: Fix Algorithm12017-10-10 10:05:20: Supplicant State:ASSOCIATING2017-10-10 10:05:20: Supplicant State:ASSOCIATED2017-10-10 10:05:20: 'WIFI_TEC' : Network Disconnected2017-10-10 10:05:20: Supplicant State:COMPLETED2017-10-10 10:05:21: 172.25.103.1:HTTP_OK:1003ms2017-10-10 10:05:21: Current dBm:-562017-10-10 10:05:21: WFMonitor Acquiring Wake Lock2017-10-10 10:05:21: Network Check:2017-10-10 10:05:21: 172.25.103.1:HTTP_OK:8ms2017-10-10 10:05:22: Current dBm:-562017-10-10 10:05:22: WFMonitor Releasing Wake Lock2017-10-10 10:05:28: Demoting network'WIFI_TEC' to 612017-10-10 10:05:36: Network Check:2017-10-10 10:05:36: 172.25.103.1:HTTP_OK:40ms2017-10-10 10:05:36: Current dBm:-562017-10-10 10:05:36: Alarm Intent2017-10-10 10:05:56: Network Check:2017-10-10 10:05:56: 172.25.103.1:HTTP_OK:8ms2017-10-10 10:05:56: Current dBm:-562017-10-10 10:06:16: Network Check:2017-10-10 10:06:16: 172.25.103.1:HTTP_OK:41ms2017-10-10 10:06:16: Current dBm:-572017-10-10 10:06:36: Network Check:2017-10-10 10:06:36: 172.25.103.1:HTTP_OK:39ms2017-10-10 10:06:36: Current dBm:-562017-10-10 10:06:56: Network Check:2017-10-10 10:06:56: 172.25.103.1:HTTP_OK:7ms2017-10-10 10:06:56: Current dBm:-562017-10-10 10:07:16: Network Check:2017-10-10 10:07:20: Network check failed: Trying again2017-10-10 10:07:20: I/O Exception172.25.103.1:HTTP_FAIL:4007ms2017-10-10 10:07:20: Current dBm:-562017-10-10 10:07:20: WFMonitor Acquiring Wake Lock2017-10-10 10:07:20: Running Wifi Repair2017-10-10 10:07:20: Reassociating2017-10-10 10:07:20: WFMonitor Releasing Wake Lock2017-10-10 10:07:20: Fix Algorithm12017-10-10 10:07:20: Supplicant State:ASSOCIATING2017-10-10 10:07:20: Supplicant State:ASSOCIATED2017-10-10 10:07:21: 'WIFI_TEC' : Network Disconnected2017-10-10 10:07:21: Supplicant State:COMPLETED2017-10-10 10:07:21: 172.25.103.1:HTTP_OK:1004ms2017-10-29 6:04 AM
Please test the FW3.5.3 (latest, online), and use the wifi_add_tim_ie/wifi_dtim_period variables (0/1 to dis/enable traffic information map information element).
If also this release is not working, I assume it's something related to powersave of P8. SPWF01 miniAP is not currently supporting powersaving STAs.
2017-10-30 2:42 AM
Thank You very much but I've just tested the 3.5.3 changing the variables above, but without results.
The distributor sent me a beta versione of firmware: SPWF01S-170213-7f49131-RELEASE-main and it works very well with P8 Lite but I'm waiting for the official release of it (I've some dubts with samsung galaxy S7). What's the differences between the two.
Thank You in advance
2017-10-30 3:50 AM
I'll be waiting for next release. I hope as soon as possible please.
Thank you very much.
2017-10-30 4:21 AM
You got a beta version of next release, allowing the module in miniAP to support powersaving STAs. Stay tuned.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.