2016-01-25 7:37 AM
Hello,
I have bought 2 SPSGRF-868-Nucleo module. I want for beginning sent a packet for see how spirit1 works. But afters some search, I don't know if my packet is really sent or not because I receive anything. I have configured 1 module for do a TX and other for RX. TX seems work, because when I sent a packet the interrupt for TX data sent is SET. For RX, I have no interrupt request for RX data available. Only discard. This discard says that the RX timeout is done. I have configured my module with this parameter :// To define :
#define XTAL_FREQUENCY 50e6
#define FREQUENCY_OFFSET 0
#define POWER_DBM 6
/* SRadioInit struct */
#define XTAL_OFFSET_PPM 0
#ifndef IF_DEF_RX
#define BASE_FREQUENCY 868000000
#else
#define BASE_FREQUENCY 868480000
#endif
#define CHANNEL_SPACE 20e3
#define CHANNEL_NUMBER 0
#define MODULATION_SELECT FSK
#define DATARATE 38400
#define FREQ_DEVIATION 20
#define BANDWIDTH 5e3
/* PktbasicInit struct */
#define PREAMBLE_LENGTH PKT_PREAMBLE_LENGTH_01BYTE // Nb de séquence 01010101
#define SYNC_LENGTH PKT_SYNC_LENGTH_4BYTES // Nombre d'octet pour la synchronisation
#define SYNC_WORD (uint32_t)0x1212000000001212 // TO DO : get à UID du STM32
#define LENGTH_TYPE PKT_LENGTH_VAR
#define LENGTH_WIDTH 0
#define CRC_MODE PKT_NO_CRC
#define CONTROL_LENGTH PKT_CONTROL_LENGTH_1BYTE
#define EN_FEC (SpiritFunctionalState)S_DISABLE
#define EN_WHITENING (SpiritFunctionalState)S_DISABLE
/*PktBasicAddressesInit struct */
#define EN_FILT_MY_ADDRESS S_DISABLE
#ifndef IF_DEF_RX
#define MY_ADDRESS 0x21
#else
#define MY_ADDRESS 0x12
#endif
#define EN_FILT_MULTICAST_ADDRESS S_DISABLE
#define MULTICAST_ADDRESS 0xFE
#define EN_FILT_BROADCAST_ADDRESS S_DISABLE
#define BROADCAST_ADDRESS 0xFF
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.