2022-05-06 12:50 AM
Hi,
Hardware used: STM32L152RE nucleo board and SPSGRF-868 module
Technology and OS: 6lowpan and Contiki.
Example used: UDP-sender and UDP-receiver.
SDK used: Sub-1 GHz RF communication software expansion for STM32Cube
I'm developing 6lowpan network using SPIRIT1, where one receiver and 10-12 sender. sender is battery operated, so I need to discover UDP receiver address(ipv6) in as short time as possible then send data.
UDP sender is using serverg-hack application to get receiver ipv6 address, it works but it takes 1-2 minutes.after that it sends data to receiver. all i need is to reduce that address detection time. or suggest me a better method.
Using SDK example path
/STM32CubeExpansion_SUBG1_V3.3.0/Projects/STM32L152RE-NUCLEO/Applications/Contiki/SPIRIT1
Thanks in advance.
Chand Bhadaniya
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.