2015-05-13 3:42 AM
Hi,
Which PA configuration parameters should I use in order to get the maximum output power on Spirit1 and which CWC (0 - 1.2 - 2.4 - 3.6 pF) bit field should be set for 868 MHz band?According to the datasheet the max output power is +11dBm or +16dBm for two different test condition. Then in the registers table it is +12 dBm for the PA_LEVEL_7. This is the highest level for the highest power. Which value should be set to POWER_DBM for max output power? I use 868MHz band with range extender. I perform the communication with GFSK_BT1 modulation at 115200 datarate. Best regards2015-05-14 3:21 AM
Hello,
In the SPIRIT1, the max RF output power is achieved by setting PA_LEVELx = 1.In our reference kit the CWC best setting is 0.For +16 dBm, there is a specific configuration, please have a look at the User Manual UM1657 section 1.2.1 ''Boost mode''.www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00092275.pdfIf You use the range extender reference kit the max RF output power is 27 dBm.SWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.