Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BlueNRG missing LE Advertising Report Event

Posted on June 07, 2014 at 10:48I can get two BlueNRG boards connecting, one as Peripheral and one as Central, using the code in the BLE_Chat example. In this case the Central has to know in advace the address of the Peripheral. However, when I try...

charles23 by Associate III
  • 2452 Views
  • 5 replies
  • 0 kudos

SPWF01XX Firmware Upgrade (usart)

Posted on April 25, 2015 at 07:20HelloI need to update the firmware (need the 1 command the is in release 3.3)for the above module. I have contacted the local ST agent and have received the required programs and files for the upgrade (via usart)(SPW...

Spirit1 PA Configuration

Posted on May 13, 2015 at 12:42Hi,Which PA configuration parameters should I use in order to get the maximum output power on Spirit1 and which CWC (0 - 1.2 - 2.4 - 3.6 pF) bit field should be set for 868 MHz band?According to the datasheet the max o...

hacer by Associate II
  • 1534 Views
  • 1 replies
  • 0 kudos

details are needed for HAL_LE_TX_TEST_PACKET_NUMBER

Posted on April 17, 2015 at 22:20In AN4494, Bring up BlueNRG app note, both Chapter 8 and 9 mention thatSend a further command to determine the number of packets sent by the Tx board: HAL_LE_TX_TEST_PACKET_NUMBER What is the LE command above? Where...

hui by Associate II
  • 1259 Views
  • 1 replies
  • 0 kudos

aci_l2cap_connection_parameter_update_request

Posted on May 08, 2015 at 17:19Hello, Please help me to clarify the following question: my device supports a several modes and I need set  special connection parameters for each mode first mode - aci_l2cap_connection_parameter_update_request(handle,...

What is ECODE 0x0001

Posted on May 10, 2015 at 14:52Hello,the very first response I get when communicating with a BlueNRG is the following byte sequence: 0x4, 0xff, 0x3, 0x1, 0x0, 0x1If I get it right, I have to read it like this:0x04 == HCI Event Packet0xff == Event Co...

torsten2 by Associate II
  • 1142 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.