2019-11-27 6:23 AM
Is there an example to see how to use the I2C inside a TouchGFX application ?
I have found the following functions but how to select the target I2C port because
I have 4 i2C ports on my 32F746G-DISCO.
I don't know which is the I2C port number for the CN2 connector.
I2C_HandleTypeDef i2c_handler;
I2Cx_Init(&i2c_handler);
I2Cx_WriteData(0x20), 0x11, 0x00);
2019-11-27 11:11 AM
Found the solution, add in the file stm32746g_discovery.c these functions and the relative declaration in stm32746g_discovery.h (...\Drivers\BSP\STM32746G-Discovery).
void BSP_I2C_Init()
{
#define I2C_ADDRESS 0x3c
#define I2C_TIMING 0x00B1112E
hi2c1.Instance = I2C1;
hi2c1.Init.Timing = I2C_TIMING;
hi2c1.Init.OwnAddress1 = I2C_ADDRESS;
hi2c1.Init.OwnAddress1 = 0x78; // an unused address
hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c1.Init.OwnAddress2 = 0;
hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
I2Cx_Init(&hi2c1);
}
void BSP_I2C_Write(uint8_t Addr, uint8_t Reg, uint8_t Value)
{
I2Cx_WriteMultiple(&hi2c1, Addr, (uint16_t)Reg, I2C_MEMADD_SIZE_8BIT, (uint8_t*)&Value, 1);
}
2019-11-28 1:18 AM
The first fuction will be called in the screen file Screen1View.cpp
void Screen1View::setupScreen()
{
#ifdef SIMULATOR
printf("LED on\n");
#else
BSP_LED_Init(LED_GREEN);
BSP_I2C_Init();
BSP_I2C_Write(0x20, 0x11, 0x00);
#endif
and the other function in the relative action
void Screen1View::buttonOPTClicked()
{
touchgfx_printf("buttonOPTClicked \n");
#ifdef SIMULATOR
printf("OPT\n");
#else
BSP_I2C_Write(0x20, 0x04, 0x30 + 1);
#endif
buttonPCM.invalidate();
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.