2019-11-26 4:43 AM
Hello !
I use a NUCLEO L152RE combined with S2LP eval board (X-NUCLEO-S2868A1). I managed to successfully register the node thanks to the S2-LP_Sigfox_DK. I'm in France so I used RC1. Then I could send some message to the sigfox backend. That's great ! :grinning_face:
Now I would like to build my own application. Here's what I did first :
I downloaded STM32CubeExpansion_SFXS2LP_V1.1.0.
I flashed my setup with Sigfox_PushButton_L1.bin. I pushed the button but could not get any new message on the sigfox backend
I then flashed my setup with Sigfox_CLI_L1.bin. Surprisingly, this time, when I pushed the button, I did receive the button count on the sigfox backend !
Does Sigfox_CLI_L1.bin contains the PushButton code ?
I'm also wondering why Sigfox_PushButton_L1.bin does not seem to work...
Then I tried to open the PushButton project in SW4STM. But I get compile issues :
fatal error: radio_shield_Config.h: No such file or directory mcu_api.c /NUCLEO_L1_ALL/Middlewares/Sigfox_STM32 line 46 C/C++ Problem
Also I find not really convenient to use SW4STM. I would prefer building with a simple Makefile. CubeMX does this. But apparently, the S2-LP is not integrated in CubeMX...
Is there simple way to build a S2-LP sigfox PushButton exemple, using a Makefile and CubeMX ?
Thanks in advance !
Pierre
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.