2019-05-08 6:43 AM
Hi,
I'm using EVK (STEVAL-FKI868V2), loading the Binaries file to EVK All the command line function is ok. but when I use your sample code:
File Location:
C:\Program Files (x86)\STMicroelectronics\S2-LP_SigFox_DK_1.6.0\Projects\Projects_Cube\S2-LP_SigFox_DK\SigFox_CLI_Demo_Project\STM32\MDK-ARM\SigFox_CLI_Demo_Project.uvprojx
That will go to "Hardware fault handler" when I type the Command line: "node_open".
is it anything difference between sample code and the Binaries file?
How can I fix this?
thanks,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.