Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

S2-LP CubeMX integration ?

Hello ! I use a NUCLEO L152RE combined with S2LP eval board (X-NUCLEO-S2868A1). I managed to successfully register the node thanks to the S2-LP_Sigfox_DK. I'm in France so I used RC1. Then I could send some message to the sigfox backend. That's great...

Hi, We got troubles to run the ST7540 power line modem "Remote Console GP PLM moudle - Rel 5.5" software.

The software crashes every time and doesn't run at all. the software installed on 6 different computers via the STEVAL-IHP005V1_Setup.exe a few times (windows xp,7,8,10). Is there any solution for this problem?We were able to successfully install and...

Query Regarding TESEO-LIV3F module. 1.Does TESEO-LIV3F provide location/Geofence Event in Basement ? If yes ,what is Accuracy ? 2.What is the process time to get the response of configurable area command ? 3.Can it support up to 200 configurable area?

We want to develop our Product in which want to use TESEO-LIV3F Chip but still we have some query so please provide proper answer quickly.1. Does TESEO-LIV3F provide location/Geofence Event in Basement ? If yes then what is the accuracy of it ?2. As ...

Running a BLE mesh demo in STEVAL-BLUEPLUG1

Hi ,I would like to run a BLE mesh demo application in the STEVAL-BLUEPLUG1 evaluation board.Two or more sensor connnected to a network publishing a stubbed value periodically.I can see from the documentation that source code is provided by ST but i ...

AM.1344 by Associate
  • 846 Views
  • 0 replies
  • 0 kudos

BlueNRG-MS not working properly

Hello everyone,I'm currently developing a custom PCB with the reference design of the STEVAL-WESU1 and I'm having problems making the BLE work. I can communicate with the chip and it answers correctly, but when told to generate the generate the servi...

0690X00000ArwiCQAR.jpg
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.