cancel
Showing results for 
Search instead for 
Did you mean: 

RF channel frequency settings for S2LP

H..10
Associate II

I am in the process of migrating from spirit1 to S2LP, I am stuck in the calibration of the frequency, before in spirit 1 it is mentioned in the datasheet of spirit1 via equation 3 

  • fc=fbase+foffset+(fxo/2^15  ×CHSPACE)×CHNUM

On the other hand in the S2LP datasheet in equation 6 it's mentionned =>

  • fc=fbase+(fxo/2^15  ×CHSPACE)×CHNUM

So I want to know where is the foffset on the S2LP equation 6

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Winfred LU
ST Employee

The offset frequency is a correction term which can be set to compensate the crystal inaccuracy after e.g. lab calibration.

Please refer to equation 7 -

foffset = (fxo / 2^18) * FC_OFFSET

where:

FC_OFFSET is a 12-bit integer (expressed as 2's complement number) set by the FC_OFFSET[1:0] registers

Winfred LU
ST Employee

For S2LP, the frequency offset is not calibrated with registers. So foffset is not shown.

H..10
Associate II

Thanks for your reply Winfred, so if the frequency offset is not calibrated with registers, is there a software workaround to fix this issue ? it means is there an alternative solution ?

Winfred LU
ST Employee

The crystal shall be calibrated in hardware.

Then the compensation can be done firmware, by measuring frequency differences on a generating single wave and configure accordingly.

This is used for most communication protocols such as Sigfox.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.