2024-04-05 6:55 AM
These answers say that the BlueNRG-M2SP module comes blank and must be programmed with a firmware binary.
How do you recommend the BlueNRG-M2SP module be programmed in a production environment? For example, are there tools available for pre-programming the module before it's soldered to the custom board? Or does the module need to be programmed in circuit through the module's SWD connection with tools such as ST-Link V2 and the programmer application? Programming in-circuit with ST-Link might be OK for low volume production but is there a better solution for high-volume products?
2024-04-05 7:17 AM
I think, ST can offer devices programmed to you spec. And there are 3-rd parties that can program for you. Otherwise to the pogrammin during boar test.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.