Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IM69D130 interface of with STM32WB55RG.

Hi STMicrocontroller developer community,I am currently working on a project that involves interfacing of infineon IM69D130 digital MEMS microphone with STM32WB55G microcontroller. However, I am facing challenges in setting up the communication betwe...

Maniksb09 by Associate II
  • 6915 Views
  • 8 replies
  • 0 kudos

Sensortile.boxpro Bluetooth

Hello everyone, I'm using a STEVAL-MKBOXPRO connected to an RPi3B+ to receive data via Bluetooth.The BLESensors code is integrated into Sensortile.I've tried two approaches and for now I'm stuck:Using the BlueSTSDK library, I've run example_ble_1.py ...

Frabbit by Associate III
  • 1274 Views
  • 0 replies
  • 0 kudos

Resolved! Heart beat signal.

Hi, MURALI SELVAM from India. I using "STM32H743VIT6" I want know heart beat signal hardware configuration, in the project I using three MCU for safety purpose, in case 1st MCU will get failure, 2nd one is take control, 2nd one will get  failure, 3rd...

murali by Associate III
  • 5981 Views
  • 9 replies
  • 0 kudos

STEVAL-MKBOXPRO and BlueST-SDK

Hi everybody, I'm a newby of ST development boards and I'm trying to use the BlueST-SDK for Python to get the data sent by the STEVAL-MKBOXPRO on the BLE interface. The python library is running on a Raspberry Pi 4 Model B, hosting on it a Python ins...

francus76 by Associate III
  • 1365 Views
  • 0 replies
  • 0 kudos

Did I brick my BlueNRG?

i have 2 STEVAL-BCN002V1B boardsthe first one i tried using the app and using bluetooth and the daughterboard (sensor board) showed solid green and i can't bluetooth connect to it and using firmware updater with USB doesnt erase to load new firmwaret...

0693W00000aIGiTQAW.png 0693W00000aIGiiQAG.jpg 0693W00000aIGixQAG.jpg 0693W00000aIGinQAG.jpg
BShal.1 by Associate II
  • 2264 Views
  • 3 replies
  • 1 kudos

Resolved! STUSB1602 register definitions and I/O line control

Hi, I need a comprehensive description of STUSB1602 registers to see if there's a possibility to control the I/O lines with them. I checked the git repository of firmwares and found something but I'd like to get a general description of the registers...

HardyFIN by Associate
  • 1718 Views
  • 3 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.