2019-11-19 5:02 AM
We want to develop our Product in which want to use TESEO-LIV3F Chip but still we have some query so please provide proper answer quickly.
1. Does TESEO-LIV3F provide location/Geofence Event in Basement ? If yes then what is the accuracy of it ?
2. As per Datasheet "Teseo-LIV3F receiver supports at least 8 circular areas where 4 circular areas are configurable in the firmware" it supports 4 configurable area but, we need to check total 200 area using our product so can we use this chip?
3. What is the process time to get the response of configurable area command ?
2019-11-19 7:42 AM
GPS/GNSS signals don't penetrate buildings/structures well, this is usually achieved via the kinetic part of the delivery system.
With 200 areas you're probably going to need to code/optimize your own solution with a micro-controller. Depending on your merit as a customer you might have access to an application layer where you can implement your own algorithm. Circles tend to be use as there are good optimization and computation reduction methods.
2019-11-19 8:52 PM
Thanks for reply.
What is the process time to get the response of configurable area command ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.