2017-07-13 3:06 AM
Hello all,
I am new using the bluenrg-1, I would like to create an application to download into the ble module but not really sure from where to start, how to do it.
I have done some test communicating with the ble using uart to send commands and it is working but now as I said I would like to download an app to just blink a led connected to one of the gpio.
Can someone help with this.
Thank you in advance
2017-07-14 1:50 AM
I have done different test, I have flashed the DTM_UART_32MHz.hex into the ble and I have seen that it is working, now I have created a small program and flash it but it seem that it is doing anything. I just want to switch on a LED, this is the code just in case I am missing something.
void main(void)
{ SystemInit();IO_Config();
while ( 1 )
{ GPIO_ToggleBits ( GPIO_Pin_1 ); DelayMs(500); }}void IO_Config ( void )
{ GPIO_InitType GPIO_InitStructure;GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1;
GPIO_InitStructure.GPIO_Mode = GPIO_Output; GPIO_InitStructure.GPIO_HighPwr = FALSE; GPIO_InitStructure.GPIO_Pull = FALSE;GPIO_Init( &GPIO_InitStructure );
}
Thanks
2017-07-14 1:59 AM
Hi,
you can use the
software package. You will find many BLE-specific examples in the Project\BLE_Examples folder. If you are interested in examples dealing with the BlueNRG-1 peripherals, instead, please refer to the Project\BlueNRG1_Periph_Examples folder. For example, you will find sample code to use the GPIO pins in Project\BlueNRG1_Periph_Examples\GPIO.Hope that helps,
Antonio
2017-07-14 4:33 AM
Hi Antonio,
I have tried the GPIO example but not having any luck with it. I can't switch on the LED.
Thanks
2017-07-14 5:22 AM
Could be possible that the cold start configuration from the
DTM_UART_32MHz.hex is different from the GPIO example? And for some reason the DTM works and not the GPIO?
Thanks
2017-07-18 2:02 AM
Maybe
Marchese.Graziella
has some additional hints to help you overcome your issue.Best regards,
Antonio
2017-07-20 7:50 AM
Hello,
It is working finally, I had a problem with the cold configuration, now I have tested the peripherals and they are working correctly. Now I'm going to test the BLE.
I am not sure, do I need to use the files inside \BlueNRG-1_2 DK 2.5.0\Library\Bluetooth_LE\inc and the library in \BlueNRG-1_2 DK 2.5.0\Library\Bluetooth_LE\library
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.