2018-01-09 9:33 AM
Hello all
I have a idw01m1 connected to f401
All seems well with the set up and I am trying to load into the flash some web pages following Lab6 instructions
I have finally found the correct cygwin to form the outfile.
typing at+s.httpdfswrite=19540 cr data.
The module declares crc errors
I take it that I have got the data length wrong (taken from file properties in windows)
Has any body got a suggestion as to what I am doing wrong please.
Andrew
2018-01-10 1:41 AM
From module's point of view:
- use flow control (mandatory to start&stop transmission while writing into flash)
- use same image needed by OTA update (httpfsupdate command)
- use 'Size' length; do not use 'Size on disk' length (for Win users)
- send image as binary file (check this flag on PC tool, if any)
This is enough I think
2018-01-10 11:42 AM
thanks for the reply Gerado,
I have spent a couple hours to no avail.
This is the set up I am using.
Teraterm com3 115200 hardware flow control, 1ms between caracters.
sending file with binary selected.
outfile properties as reported by windows size 19k (19.540) size on disc 20k (20480)
2018-01-11 5:52 AM
OK for flowcontrol between PC and STM32 (idw01m1 application). Please be sure that flowcontrol enabled between STM32 and SPWF01 too (there is a configuration variable to be set onto module).
STM32CubeExpansion_WIFI1_V3.1.1? Are you using WiFi_VCOM application? Which target platform (STM32)?
2018-01-11 11:15 AM
That must be it then I have been trying to do this from pre compilled version
Now I have loaded the files in to system work bench.
But to save me some time can you point me in the right direction for change to be made
Regards Andrew
main board nucleoF401RE
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.