2019-08-23 9:09 AM
I wrote a version with 16 bit UUIDs, but it seems that LightBlue doesn't handle duplicate UUIDs in the same service (Service: Automation I/O; I added 4 analogs and 3 digitals; some are R/O and some are R/W, but LightBlue only is using the permissions of the first UUID in the service), so I changed it to 128 bit UUIDs.
Now, about 3/4 of the way through setting up the characteristics, I'm getting a 0x48 back from the aci_gatt_add_char call...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.