Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

B-LCDAD-HDMI1 i2c address change from default

I have the B-LCDAD-HDMI1 and the datasheet says it's "default" i2c address is 0x7a. the ADV7533 datasheet says the i2c address is determined by the PD pin on power-up. what I can;lt find is what the i2c address can be changed to. Does anyone kno...

FCC Standards S2LP parameters for 902 – 928 MHz

Hi. is there any example using  902 – 928 MHz just using S2LP(no Sigfox), which fulfill the FFC standards regarding to the frequency hopping. according to AN4949, my understanding , in SRadioInit base frequency would be 902 Mhz with frequency de...

Jutt by Associate II
  • 773 Views
  • 0 replies
  • 1 kudos

Is there a limit to the number of characteristics in the BlueNRG-1, and is it dependent on UUID length?

I wrote a version with 16 bit UUIDs, but it seems that LightBlue doesn't handle duplicate UUIDs in the same service (Service: Automation I/O; I added 4 analogs and 3 digitals; some are R/O and some are R/W, but LightBlue only is using the permissions...

TJohn.14 by Associate II
  • 734 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.