2019-08-23 9:18 AM
Is there a guidance sheet for the BlueNRG_Stack_Initialization_t structure passed into BlueNRG_Stack_Initialization?
I've been using the SensorDemo application as a template, and found that I need to say
#define MAX_NUMBER_ATTRIBUTE_SERVICE1 (13)
Even though the first service (DeviceInfo) is only using 4 characteristics...
Best I can figure is that it should be 3*Nchar+1 (for the service entry)... if it's made too much larger, it fails, and if it's made smaller, you start getting errors when you call aci_gatt_add_char.
But why *3?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.