2019-01-07 2:48 AM
Hi everyone,
I try to implement the stack Bluetooth 4.2.0 X-CUBE-BLE1 with the sensorDemo application on a Nucleo-L452RE evaluation kit, coupled with X-NUCLEO-IDB05A1 Bluetooth Board.
The code C has been generated thanks to STM32CubeMX 5.0.0 standalone with the help of the manual "UM1873: Getting started with the X-CUBE-BLE1 Bluetooth Low Energy software expansion for STM32Cube".
The compilation is realized thanks to the ac6 OpenSTM32 (Eclipse + gcc-arm).
When the code is implemented with no others modifications, the bluetooth module doesn't work. After investigation by a step-by-step running, it appears the initialisation is not finalised: the software goes to nowhere land once the SPI reset is realized (hciContext.io.Reset() of the hci_init function). I would have the feeling the software stays somewhere in interrupt. I have found, also, a weirdo thing: the SPI and UART initialisation functions don't appear in the CubeMx generated code. I tested to add manually the SPI and UART init functions, but the problem stays identical.
The problem stays also identical with the compilation of the code provided by ST:
https://www.st.com/en/embedded-software/x-cube-ble1.html
Anyone would have any ideas?
2022-07-09 3:56 PM
How did you fix this problem?
I am using the X-NUCLEO-IDB05A2 with same nucleo board.
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.