2022-07-11 5:59 PM
I am using a BlueNRG-LP MC355 SoC. When connected to my debugger, I can call NVIC_SystemReset() just fine. However, if I disconnect the debugger, the device hard faults on reset.
uint8_t ret = BLE_STATUS_SUCCESS;
uint16_t service_handle, dev_name_char_handle, appearance_char_handle;
static uint8_t adv_data[] = {0x02, AD_TYPE_FLAGS, FLAG_BIT_LE_GENERAL_DISCOVERABLE_MODE | FLAG_BIT_BR_EDR_NOT_SUPPORTED,
6, AD_TYPE_COMPLETE_LOCAL_NAME, 'H', 'O', 'W', 'D', 'Y'};
/* Set the TX power 0 dBm */
aci_hal_set_tx_power_level(0, 24);
/* GATT Init */
ret = aci_gatt_srv_init();
if (ret != BLE_STATUS_SUCCESS)
{
PRINTF("aci_gatt_srv_init() failed: 0x%02x\r\n", ret);
return ret;
}
/* GAP Init */
ret = aci_gap_init(GAP_PERIPHERAL_ROLE, 0, 0x07, STATIC_RANDOM_ADDR, &service_handle, &dev_name_char_handle, &appearance_char_handle);
if (ret != BLE_STATUS_SUCCESS)
{
PRINTF("aci_gap_init() failed: 0x%02x\r\n", ret);
return ret;
}
/* Update device name */
Gap_profile_set_dev_name(0, sizeof(device_name), device_name);
ret = aci_gap_set_authentication_requirement(BONDING,
MITM_PROTECTION_REQUIRED,
SC_IS_NOT_SUPPORTED,
KEYPRESS_IS_NOT_SUPPORTED,
7,
16,
USE_FIXED_PIN_FOR_PAIRING,
123456);
if (ret != BLE_STATUS_SUCCESS)
{
PRINTF("aci_gap_set_authentication_requirement()failed: 0x%02x\r\n", ret);
return ret;
}
// HARD FAULT HAPPENS HERE
ret = aci_gap_set_advertising_configuration(0, GAP_MODE_GENERAL_DISCOVERABLE,
ADV_PROP_CONNECTABLE | ADV_PROP_SCANNABLE | ADV_PROP_LEGACY,
(ADV_INTERVAL_MIN_MS * 1000) / 625, (ADV_INTERVAL_MAX_MS * 1000) / 625,
ADV_CH_ALL,
0, NULL,
ADV_NO_WHITE_LIST_USE,
0, /* 0 dBm */
LE_1M_PHY, /* Primary advertising PHY */
0, /* 0 skips */
LE_1M_PHY, /* Secondary advertising PHY. Not used with legacy advertising. */
0, /* SID */
0 /* No scan request notifications */);
PRINTF("Advertising configuration 0x%02X\n", ret);
ret = aci_gap_set_advertising_data(0, ADV_COMPLETE_DATA, sizeof(adv_data), adv_data);
PRINTF("Set advertising data 0x%02X\n", ret);
PRINTF("BLE Stack Initialized with SUCCESS\n");
// init services here
services_init();
}On reset, without a debugger connected, I cannot get passed `aci_gap_set_advertising_configuration()`...
My config file is almost exactly like the BLE_Sensor_Demo:
My intention was to create a BLE characteristic that when written would reset the device:
/* .... */
/* Device information characteristic definition */
static ble_gatt_chr_def_t chars[] = {
{/* Reset characteristic */
.properties = BLE_GATT_SRV_CHAR_PROP_WRITE | BLE_GATT_SRV_CHAR_PROP_WRITE_NO_RESP,
.permissions = BLE_GATT_SRV_PERM_NONE,
.min_key_size = BLE_GATT_SRV_MAX_ENCRY_KEY_SIZE,
.uuid = BLE_UUID_INIT_16((RESET_UUID)},
};
/* WOWL service definition */
static ble_gatt_srv_def_t service = {
.type = BLE_GATT_SRV_PRIMARY_SRV_TYPE,
.uuid = BLE_UUID_INIT_16SERVICE_UUID),
.chrs = {
.chrs_p = chars,
.chr_count = 1u,
},
};On write to that characteristic, I simply call `NVIC_SystemReset()`. Any help appreciated.
@Sebastien DENOUAL @Winfred LU , Thoughts? What am I missing?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.