2017-04-25 10:24 PM
Hello!
I recently bought the IDW01M1 WiFi expansion board
and I am trying to have it working with the STM32F411RE.
However, from the examples in en.x-cube-wifi1_firmware.zip,
I can find the .bin file for STM32F401RE-Nucleo only
and so I tried to flash this WiFi_VCOM .bin to the STM32F411RE board.
I can see LED1 is green, so power is ok.
No other LED On, so module is ok?!
When I use Tera Term, I don't see any output and when I send 'AT', no 'OK' either.
So my question is that F401RE .bin image cannot work directly on F411RE board please?!
Since I am still a newbie to this WiFi module, I am not sure if it will be easy to recompile the sample application for F411RE then?!
Any suggestion / comment is welcome.
Thanks & Best Regards,
Robert
#stm32f411re-wifi-idw01m12017-06-12 12:02 PM
Thanks, Jerry.
I tried but it's still not working yet
and so I think that the UART driver difference may be the other source of problem to be debugged next...
In fact, I don't get any of the Wifi Indication message displayed at all
but I know that my Wifi initialization is still ok because I received the hardcoded data I sent.
So I suspect that the mixing of UART driver code is causing both the Wifi Indication message problem and my usart_print() problem now...
Thanks & BR,
Robert
2018-01-28 10:52 AM
Hi
Das.Mridupawan
,I tried your way to convert from F401RE to F411RE Nucleo but it failed. There is an error in file
stm32f4xx_ll_dma.h
Error[Pe020]: identifier 'DMA_SxM1AR_M1A' is undefined D:\Outstanding STM32\STM32CubeExpansion_WIFI1_V3.1.1\Drivers\STM32F4xx_HAL_Driver\Inc\stm32f4xx_ll_dma.h 1621
I used the HTTP_Request example. Can you have a little look it it? Thank you so much. I think IAR is the most simple way to convert from F401RE to F411RE. I tried with Keil but it failed.
Best regards,
Duy
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.