2020-02-25 3:32 AM
Hello everyone,
I just got an IDB008v2 evaluation board and I'm having some issues setting it up and programming it.
I can flash some demo programs from the BlueNRG-2 Navigator, which works (Tera Term receives the print messages and BLE scanner app sees the advertising). But if I load the same demo programs in Keil uVison5 (build successful) and try to flash it, I get the error message "No ST-LINK" detected.
In the target options, device tab, the device is correctly identified as BlueNRG-2.
I tried connecting using the BlueNRG-1 ST-LINK Utility, but connecting to the target yields the same error: "No ST-LINK detected". I tried disconnecting/reconnecting, reinstalling the drivers, resetting the board before connecting, rebooting the computer. No change.
I'm on Windows 10
2020-03-09 2:46 AM
Hello,
I wanted to second this. It also happens on my machine. I can write programs via the Navigator, but neither with KEIL nor with the STLINK.
Tam
2020-03-09 3:01 AM
Hi Thann,
First, make sure of the following things:
I discussed with the ST tech support team privately and we found a workaround for the IDB008V2.
First, you need the BlueNRG1 ST-LINK Utility which will allow you to flash the board.
Open this utility and go to Target > Settings and set the mode to "Hot Plug". Then try to Target > Connect.
If connecting doesn't work, take a cable and bridge between a VBLUE pin and the DIO7 pin, then, in that order:
The Utility should now be able to connect to the ST-LINK. You can program in Keil or TrueStudio, then build the project. Then, go into the Utility and open the hex or bin file from your build, then you can Target > Program the board.
Unfortunately, this workaround doesn't allow you to use either KEIL's or TrueStudio's debuggers, but you can still debug with printf and see the output in a terminal like TeraTerm (make sure your serial is configured with a rate of 115200).
I hope that helps,
Bests,
Rémi
2020-03-09 3:12 AM
Hello Remi,
thank you for your detailed reply - this confirms my worst fears. It looks like it is not possible to debug the BlueNRG2 at all, at least with the ST-Link. Maybe a Segger JProbe works, but these are pricey and not so easy to buy.
Either way, I was stupid. I just connected the board using the USB cable which came with it and expected it to have an integral ST-Link like a Nucleo. This one does not - my mistake, I know, but SGS could have been clearer.
Tam
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.