2016-04-19 6:27 AM
Hi,
I am having a problem with the HTTPDFSUPDATE failing mid download here is what I see on the console: Image length 338827 (offset 0x00080000, block len 4096) Write len 4096 -> 0x8B000 Write len 4096 -> 0x8C000 Write len 4096 -> 0x8D000 Write len 4096 -> 0x8E000 Write len 4096 -> 0x8F000 Write len 4096 -> 0x90000 Write len 3227 -> 0x91000 (final) Wrote 72859 byte Error (-3 @ 72855/338828), cleaning up.. +WIND:2:Reset+WIND:1:Poweron (160129-c5bf5ceSPWF01S)
+WIND:0:Console active What does error -3 mean? I have tried both FW 3.4 & the newest FW 3.5 on the module. The point at which it stops during the download seems to vary, also it sometimes does sucessfully finish the full download. Thanks in advance.2016-04-19 7:18 AM
Hi,
-3 means timeout. Please check your webserver settings, and module ip_http_get_recv_timeout configuration variable (you can increase default value, eventually).Regardsj2016-04-22 2:22 AM
Thanks - increasing the timeout seemed to solve the issue short term. Need to check what's happening the server end and why it is so slow.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.