2024-11-13 7:11 AM - last edited on 2025-02-03 12:54 PM by Peter BENSCH
Hi,
I am trying to connect the STEVAL-BFA001V2B to a siemens ET-200SP IO-Link master. I have flashed the MCU with the STEVAL-BFA001V2_PredMaint_IOL_V1.1.0 using the STM32Cube Programmer. The PLC's IO link configurator connects with the BFA001V2B however is shows an error (0x 1800 - Event ALARM on axis X in SUB1) and (0x 180A - Event ALARM on axis Z in SUB2). I have attached images showing the errors and of the process data being all 0.
I would really appreciate any help in solving this issue.
Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.