2024-01-15 2:50 AM - edited 2024-01-15 5:46 AM
I am designing a usb type-c charger.
I want to use 2 microcontroller and 2 STUSB4710.
Type-C Output will be 20V 3.35A 67W.
I want to do power management between these USB Type-C outputs.
I have questions. Can you please answer them?
1. Are there any I2C command to close the output pmosfets with STUSB4710?
2. Can microcontroller reduce the output current capabilities of STUSB4710 while a device connected to USB Type-C sinking some current. For example,
3. Is there any other way to reduce sinking current of the connected usb device?
4. STUSB4710 supports 20V 5A. But Vconn is not supported with STUSB4710. Is there a standard incompatibility?
5. Is 20V 3.35A type-C output possible with STUSB4710?
6. I have found this post https://community.st.com/t5/interface-and-connectivity-ics/stusb4700-4710-i2c-register-details/td-p/234334. But I did not find any clear guidelines(step by step) for changing register and effects of it. Also some registers contained TBD values.
2024-02-13 10:07 AM
Hi,
we are using the STSW-STUSB006 I2C Lib whose only pupose is the programming of the STUSB4761 with an own MCU. What else does ST think what the Customers will do with it?
The datasheet explicit describes multiple reprogramming and what to do that the new configuration will take effect. Definitely not 'write once'
I assume the NVM is a normal flash with 10.000 to 100.000 write cycles.
Please clarify the maximum allowed write cycles.
It would be better if ST clearly says what this Chip can do and what not.
Not this information obscurity of unspoked things to 'protect' the customer from his own decisions he made with much to less informations.
Best Regards
Michael
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.