2022-12-05 8:57 AM
@I'm new to BlueNRG. I have choosen BLE_SerialPort_Master_Slave project for my project. I need to connected with my Master(Mobile app) and receive data from the app.
I would like to create a new service which is similar to the existng Add_SerialPort_Service(). Here I have created a new service function named Add_Travel_Service(). The code inside the travel_service is same as serialport_service function. Here I just want to see, how to create a new service. I compile and flash the hex file, I never see a new service added.
I have increased the macros in SerialPort_config.h, however no use.
/* Default number of link */
#define MIN_NUM_LINK 10
/* Default number of GAP and GATT services */
#define DEFAULT_NUM_GATT_SERVICES 10
/* Default number of GAP and GATT attributes */
#define DEFAULT_NUM_GATT_ATTRIBUTES 9
/* Number of services requests from the serial port demo */
#define NUM_APP_GATT_SERVICES 10
/* Number of attributes requests from the serial port demo */
#define NUM_APP_GATT_ATTRIBUTES 10
/* Number of links needed for the demo: 1
* Only 1 the default
*/
#define NUM_LINKS (MIN_NUM_LINK)
/* Number of GATT attributes needed for the serial port demo. */
#define NUM_GATT_ATTRIBUTES (DEFAULT_NUM_GATT_ATTRIBUTES + NUM_APP_GATT_ATTRIBUTES)
/* Number of GATT services needed for the serial port demo. */
#define NUM_GATT_SERVICES (DEFAULT_NUM_GATT_SERVICES + NUM_APP_GATT_SERVICES)
/* Array size for the attribute value */
#define ATT_VALUE_ARRAY_SIZE (44 + 80) //(GATT + GAP) = 44 + Serial Port (TX (41) + RX (39) characteristics) Services
/* Flash security database size */
#define FLASH_SEC_DB_SIZE (0x400)
/* Flash server database size */
#define FLASH_SERVER_DB_SIZE (0x400)
/* Set supported max value for ATT_MTU enabled by the application. Allowed values in range: [23:158] [New parameter added on BLE stack v2.x] */
#define MAX_ATT_MTU (DEFAULT_ATT_MTU)
/* Set supported max value for attribute size: it is the biggest attribute size enabled by the application */
#define MAX_ATT_SIZE (20)My code for the new service in gatt_db.c file is
uint8_t Add_SerialPort_Service(void)
{
uint8_t ret;
/*
UUIDs:
D973F2E0-B19E-11E2-9E96-0800200C9A66
D973F2E1-B19E-11E2-9E96-0800200C9A66
D973F2E2-B19E-11E2-9E96-0800200C9A66
*/
const uint8_t uuid[16] = {0x66,0x9a,0x0c,0x20,0x00,0x08,0x96,0x9e,0xe2,0x11,0x9e,0xb1,0xe0,0xf2,0x73,0xd9};
const uint8_t charUuidTX[16] = {0x66,0x9a,0x0c,0x20,0x00,0x08,0x96,0x9e,0xe2,0x11,0x9e,0xb1,0xe1,0xf2,0x73,0xd9};
const uint8_t charUuidRX[16] = {0x66,0x9a,0x0c,0x20,0x00,0x08,0x96,0x9e,0xe2,0x11,0x9e,0xb1,0xe2,0xf2,0x73,0xd9};
const uint8_t uuid3[16] = {0x88,0x20,0xc4,0x80, 0xe4,0x8b, 0x11,0xe2, 0x84,0x0b, 0x00,0x02,0xa5,0xd5,0xc5,0x1b};
Osal_MemCpy(&service_uuid.Service_UUID_128, uuid, 16);
ret = aci_gatt_add_service(UUID_TYPE_128, &service_uuid, PRIMARY_SERVICE, 6, &SerialPortServHandle);
if (ret != BLE_STATUS_SUCCESS) goto fail;
Osal_MemCpy(&char_uuid.Char_UUID_128, charUuidTX, 16);
ret = aci_gatt_add_char(SerialPortServHandle, UUID_TYPE_128, &char_uuid, 20, CHAR_PROP_NOTIFY, ATTR_PERMISSION_NONE, 0,
16, 1, &TXCharHandle);
if (ret != BLE_STATUS_SUCCESS) goto fail;
Osal_MemCpy(&char_uuid.Char_UUID_128, charUuidRX, 16);
ret = aci_gatt_add_char(SerialPortServHandle, UUID_TYPE_128, &char_uuid, 20, CHAR_PROP_WRITE|CHAR_PROP_WRITE_WITHOUT_RESP, ATTR_PERMISSION_NONE, GATT_NOTIFY_ATTRIBUTE_WRITE,
16, 1, &RXCharHandle);
if (ret != BLE_STATUS_SUCCESS) goto fail;
printf("Serial Port Service added.\nTX Char Handle %04X, RX Char Handle %04X\n", TXCharHandle, RXCharHandle);
return BLE_STATUS_SUCCESS;
fail:
printf("Error while adding Serial Port service.\n");
return BLE_STATUS_ERROR ;
}
tBleStatus Add_Travel_Service(void)
{
tBleStatus ret;
const uint8_t uuid1[16] = {0x66,0x82,0x1a,0x40, 0xe4,0x77, 0x11,0xe2, 0x82,0xd0, 0x00,0x02,0xa5,0xd5,0xc5,0x1b};
const uint8_t uuid2[16] = {0x77,0x2e,0x55,0x20, 0xe4,0x77, 0x11,0xe2, 0xa9,0xe3, 0x00,0x02,0xa5,0xd5,0xc5,0x1b};
const uint8_t uuid3[16] = {0x88,0x20,0xc4,0x80, 0xe4,0x8b, 0x11,0xe2, 0x84,0x0b, 0x00,0x02,0xa5,0xd5,0xc5,0x1b};
Osal_MemCpy(&service_uuid.Service_UUID_128, uuid1, 16);
ret = aci_gatt_add_service(UUID_TYPE_128, &service_uuid, PRIMARY_SERVICE, 6, &SerialPortServHandle);
if (ret != BLE_STATUS_SUCCESS) goto fail;
Osal_MemCpy(&char_uuid.Char_UUID_128, uuid2, 16);
ret = aci_gatt_add_char(SerialPortServHandle, UUID_TYPE_128, &char_uuid, 20, CHAR_PROP_NOTIFY, ATTR_PERMISSION_NONE, 0,
16, 1, &TXCharHandle);
if (ret != BLE_STATUS_SUCCESS) goto fail;
Osal_MemCpy(&char_uuid.Char_UUID_128, uuid3, 16);
ret = aci_gatt_add_char(SerialPortServHandle, UUID_TYPE_128, &char_uuid, 20, CHAR_PROP_WRITE|CHAR_PROP_WRITE_WITHOUT_RESP, ATTR_PERMISSION_NONE, GATT_NOTIFY_ATTRIBUTE_WRITE,
16, 1, &RXCharHandle);
if (ret != BLE_STATUS_SUCCESS) goto fail;
return BLE_STATUS_SUCCESS;
fail:
printf("Error while adding new service.\n");
return BLE_STATUS_ERROR ;whenever, I change the macros, I dont even find my device (undiscoverable). Can some one help me out how to add new service. Also I have edited the SerialPort_DeviceInit function in the seial_port.c file like below
uint8_t SerialPort_DeviceInit(void)
{
uint8_t ret;
uint16_t service_handle, dev_name_char_handle, appearance_char_handle;
/* Setup the device address */
Setup_DeviceAddress();
/* Set the TX power to -2 dBm */
aci_hal_set_tx_power_level(1, 4);
/* GATT Init */
ret = aci_gatt_init();
if(ret != BLE_STATUS_SUCCESS) {
PRINTF("GATT_Init failed: 0x%02x\n", ret);
return ret;
}
/* GAP Init */
ret = aci_gap_init(GAP_CENTRAL_ROLE|GAP_PERIPHERAL_ROLE, 0,0x07, &service_handle,
&dev_name_char_handle, &appearance_char_handle);
if(ret != BLE_STATUS_SUCCESS) {
PRINTF("GAP_Init failed: 0x%02x\n", ret);
return ret;
}
// Add Device Service & Characteristics
ret = Add_SerialPort_Service();
if(ret != BLE_STATUS_SUCCESS) {
PRINTF("Error while adding service: 0x%02x\n", ret);
return ret;
}
/*ret = Add_Travel_Service();
if(ret != BLE_STATUS_SUCCESS) {
PRINTF("Error while adding service: 0x%02x\n", ret);
return ret;
}*/
/* Reset the discovery context */
Reset_DiscoveryContext();
return BLE_STATUS_SUCCESS;
}Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.