Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

S2-LP How to RX IEEE 802.15.4g packet format?

How do I get the expected payload length from the PHR?The PHR isn't expected to be available after the SYNC_WORD detected interrupt so either the FIFO_RXAF threshold interrupt or RX_DATA_READY interrupt should indicate data in the RX FIFO and the len...

JKo by Associate III
  • 1231 Views
  • 1 replies
  • 0 kudos

STM32Cube programmer does not recognize SPIN3200

I'm trying to connect STEVAL-SPIN3200 with STM32Cube programmer however when I do it appears either of these message: Warning: Connection to device 0x444 is lost or Error: No STM32 target found!I've tried all different solutions but still can't conne...

CChav.1 by Associate
  • 894 Views
  • 0 replies
  • 0 kudos

STUSB4700: Power Delivery Configuration Questions

Hello,I am designing a USB-C Power Delivery circuit where our product is the source (NOT the sink). The system can be enabled/disabled via a user button, meaning the USB-C PD portion will lose its control supply power. I would like to be able to achi...

KMew by Senior III
  • 3436 Views
  • 6 replies
  • 0 kudos

BlueNRG-LP Current Consumption

Hi, I am evaluating the current consumption of BlueNRG-LP using STEVAL-IDB10V1 and i am a bit confused with the expected and actual device's currents.According to the datasheet, peak TX current during connection at 0dB is 4.3mA, according to Current ...

TLans.1 by Associate II
  • 1595 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.